Skip to main content
Associate
Aug 30, 2023 11:19 PM UTC
Question

STD80N240K6 - Electrical Characteristics

Hi,

I am doing simulations for Electrical Characteristics and find the the IDSS and IGSS are in the range of nA instead of uA as quoted in the datasheet. Can any ST Engineer help me if the numbers need updates? 

I filed a support ticket, instead was informed that I can find answers on the community forum.

Thank you for the help.

Best Regards,

Ramu

This topic has been closed for replies.

3 replies

TDK
Aug 31, 2023 12:09 AM UTC

Datasheet says 1 uA max. You don't say what you measured specifically, or your test conditions, but certainly "range of nA" is under 1 uA.

Nominal will certainly be under 1 uA, obviously.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Aug 31, 2023 4:12 PM UTC

IDSS --> Conditions ==> VDS=800V VGS=0v, Temp=25C, Corner conditions = Nominal, Fast

Simulated current in the range of nA(for both Nominal & Fast) instead of uA (Datasheet)

IGSS --> Conditions ==> VDS=0V VGS=-20v to +20v, Temp=25C, Corner conditions = Nominal, Fast

Simulated current in the range of nA(for both Nominal & Fast) instead of uA (Datasheet)

Let me know if the simulated current values are within the specifications. 

If ST can share the simulated setup, that would be helpful.

Best Regards,

Ramu

 

Associate
Sep 5, 2023 3:31 PM UTC

Any ST application/support engineers, who can review my post and provide feedback will be helpful.

Best Regards,

Ramu