Skip to main content
Associate II
Jul 14, 2026 12:42 PM UTC
Solved

ST87M01 WiFi Scan performance very weak compared to ESP32 (same antenna)

Hi all,

I'm experiencing very poor WiFi scan sensitivity with the ST87M01 (FW 2.9.0) compared to an ESP32 using the exact same antenna (connected via U.FL). While the ESP32 easily finds multiple networks, the ST87M01 only sees very few, or none at all.

Device Info & Scan Config (ST87M01)

```text
ati
STMICROELECTRONICS
ST87M01-1301
A:2.9.0-M:2.9.0-S:2.9.0-G:2.9.0-B:1.1

AT#WSCAN=4,1      <-- [Config] RF Path (NB-IoT antenna path)
OK
AT#WSCAN=3,500   
OK
AT#WSCAN=5,3     
OK
AT#WSCAN=2,0     
OK
AT#WSCAN=1,1,6,11 <-- [Action] Trigger scan on channels 1, 6, 11
OK
...
#WSSTOP           <-- [Result] (Hardly any networks returned)
```

Reference: ESP32 Scan (Same Antenna, same spot)

```text
1: Yippie (BSSID: 3C:A6:2F:B5:E4:37, Kanal: 11, RSSI: -48 dBm)
2: RAK7268V2_BAD1 (BSSID: AC:1F:09:19:BA:D2, Kanal: 11, RSSI: -50 dBm)
3: Yippie (BSSID: D4:24:DD:4D:F2:2F, Kanal: 11, RSSI: -54 dBm)
4: Yippie (BSSID: DC:39:6F:1F:5C:03, Kanal: 11, RSSI: -76 dBm)
5: linksys (BSSID: 98:FC:11:CE:00:16, Kanal: 9, RSSI: -86 dBm)
6: Yippie (BSSID: D4:24:DD:4D:F4:90, Kanal: 11, RSSI: -86 dBm)
```

Questions:
Is there an issue?

Configurations in the ST87M01 AT commands I might have missed?

Any hints on what I might be doing wrong are highly appreciated!

Thanks, Jo

Didier HERROUIN
Didier HERROUINBest answer
ST Technical Moderator
Jul 20, 2026 9:29 AM UTC

Dear GeoP,

Are you able to check if the BSSIDs you have listed are based on 801.11b or 802.11g ?
Indeed, the ST87M01 scans only the 802.11b.

Best regards,

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Andrew Neil
Super User
Jul 14, 2026 1:07 PM UTC

```text

This forum doesn’t support markdown.

You are invited to provide feedback about that here:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Didier HERROUIN
ST Technical Moderator
Jul 16, 2026 12:44 PM UTC

Dear GeoP,

Yes, there is an issue as your results are not inline with ST87M01 sensitivity.

Your settings and AT commands are correct.
Please enable URC mode by AT#WSCAN=2,1 to get a better view of the events and send back the logs.
You could also increase the scanning time : AT#WSCAN=3,1000

Which board do you use ?

  • If you use the evaluation kit “EVKITST87M01-2”, please use the antenna provided in the box and compare with your actual results.
  • If you use your own board, you should check the antenna path (do you use a 50ohms impedance track ?).
    Can you share the reference of the antenna you use ?

Best regards,

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Didier HERROUIN
Didier HERROUINBest answer
ST Technical Moderator
Jul 20, 2026 9:29 AM UTC

Dear GeoP,

Are you able to check if the BSSIDs you have listed are based on 801.11b or 802.11g ?
Indeed, the ST87M01 scans only the 802.11b.

Best regards,

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
GeoPAuthor
Associate II
Aug 27, 2026 8:56 AM UTC

Hmm, i can not check this, the lab uses a 'FritzBox 2400 Repeater', however customer has decided to not use the WiFi Scan, now he wants GNSS over LTE antenna with SAW and LNA, that works very well (as in the ST Appnote).