Skip to main content
Associate
Nov 13, 2026 10:56 AM UTC
Question

ST67W6X Disable WPS in access point mode

Hello,

 

I am using the ST67W6X module with T02 mission in one of my projects.

I am configuring the module in acess point mode, WPA2 and configure a password (10 characters).

When connecting with the iPhone, everything works well.

When connecting with the windows laptop, windows requests me to enter a 8 digit password (WPS). I have to click on a link below the password field to switch to password mode. Then I can enter the password and the connection works.

 

Question:

How can I disable the WPS advertising of the ST67W6X module when configured in access point mode?

I could not find any C API call that does this. 

 

Thanks and best regards,

Stefan

3 replies

EPASZ.1
ST Employee
Nov 13, 2026 11:41 AM UTC

Hello,

this is a known issue and will be fixed in the next version of the SDK.

For SoftAP operation, the WPS functionality should be disabled by default, with no way to use it. Only STA mode (or the STA part when operating in STA+SoftAP mode) supports WPS.

Associate
Nov 13, 2026 12:13 PM UTC

Hi,

 

thanks for the quick response!

I am glad that this issue will be resolved in the next release.

Is there any plan about when the next release will be made?

 

Best regards,

Stefan

EPASZ.1
ST Employee
Nov 13, 2026 12:37 PM UTC

As far as I know, the current target for the next release is Q1 next year.