Skip to main content
Associate
Oct 1, 2026 8:34 AM UTC
Solved

ST67W611M1 Support for IEEE 802.11k/v/r and Wi-Fi Roaming

Could you please clarify whether the ST67W611M1 supports IEEE 802.11k/v/r and Wi-Fi roaming?

If it does, could you please point me to the documentation that describes this support? I could not find any information about it in the datasheet, user manual, or ST Wiki.

TarikAbBest answer
ST Technical Moderator
Oct 1, 2026 10:24 AM UTC

Hi ​@yama4815 ,

 

The ST67W611M1 module doesn’t support hardware Wi-Fi roaming. It may be possible to attempt some SW Wi-Fi roaming implementation by monitoring the RSSI and comparing it to a user-defined value. If RSSI falls below this value, the STA would rescan and connect to the “new” AP with the same SSID and a higher RSSI. Such SW feature means of course a connection loss during the rescan.

 

Best regards,

Tarik

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

7 replies

TarikAbBest answer
ST Technical Moderator
Oct 1, 2026 10:24 AM UTC

Hi ​@yama4815 ,

 

The ST67W611M1 module doesn’t support hardware Wi-Fi roaming. It may be possible to attempt some SW Wi-Fi roaming implementation by monitoring the RSSI and comparing it to a user-defined value. If RSSI falls below this value, the STA would rescan and connect to the “new” AP with the same SSID and a higher RSSI. Such SW feature means of course a connection loss during the rescan.

 

Best regards,

Tarik

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Oct 6, 2026 9:46 AM UTC

The ST67W611M1 module doesn’t support hardware Wi-Fi roaming.

Is that a hardware limitation, or just that it’s not (yet) implemented in any module firmware?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
Oct 7, 2026 12:12 PM UTC

Not sure about where the limitation is exactly but I can say that this feature won’t be supported by the ST67W611M1 module.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yama4815Author
Associate
Oct 6, 2026 5:41 AM UTC

Thank you for your reply.
Does this mean that support for 802.11k/v/r is also not available?
Thank you in advance.

ST Technical Moderator
Oct 6, 2026 12:27 PM UTC

This is correct.

If possible, could you share more details on the use-case requiring the support of 802.11 k/v/r?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
yama4815Author
Associate
Oct 12, 2026 11:54 PM UTC

Thank you for your response.

I had in mind equipment that communicates while in motion and, by design, cannot tolerate even a momentary loss of connectivity.

Andrew Neil
Super User
Oct 13, 2026 8:50 AM UTC

What kind of equipment?

And what kind of environment do you envisage providing such seamless coverage?

 

Even cellular cannot guarantee that you will never experience “even a momentary loss of connectivity” - a mobile device really needs to be able to tolerate that!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.