Skip to main content
3FTI
Associate III
Aug 11, 2026 7:24 PM UTC
Solved

ST67W61 Target-Wake-Time sample project

Is there a demonstration project (outside of the CLI) for the target-wake-time feature?

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Sep 1, 2026 9:49 AM UTC

Hello ​@3FTI ,

Actually, the TWT is only exercised in the CLI project, as this feature is dependent of the configuration of the access point you're connected to.

You can test it on the Echo or HTTP client project for example.

Regards
Louis

1 reply

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Sep 1, 2026 9:49 AM UTC

Hello ​@3FTI ,

Actually, the TWT is only exercised in the CLI project, as this feature is dependent of the configuration of the access point you're connected to.

You can test it on the Echo or HTTP client project for example.

Regards
Louis