ST Link V3 cannot connect to BlueNRG2 when running FreeRTOS
- 3 replies
- 1656 views
I noticed a peculiar issue regarding FreeRTOS and ST Link. If you flash the BLE Beacon FreeRTOS example into the development board, ST Link cannot connect or event detect the BlueNRG target. This happens both with BlueNRG-X Flasher Utility and in Keil uVision. Only way to regain connection is to flash non-FreeRTOS example using BlueNRG-2 Navigator.
If I build and start a debug session with a FreeRTOS project, the target is flashed correctly, but almost immediately when entering main the connection is lost. This happens even if all FreeRTOS calls are removed.
In the attachments you can find log file where I flashed a FreeRTOS binary into the development board two times a row. The first flash is successful, but there is immediately a failure when ST Link tries to disconnect from the target. The next flashing fails immediately.
Any idea what could be causing this? What the FreeRTOS image is doing so that it kills the SWD?