Skip to main content
FSchm.1
Visitor II
Aug 25, 2020 8:23 AM UTC
Question

SPWF04S MQTTCONN Request Failed

Hi together,

I'm using the NUCLEO-F401RE and NUCLEO-IDW04A1 trying to connect and publish to a MQTT Broker. Therefore i've edited the example HTTP_Request. Connecting to my WiFi-AP is working fine, but connecting to the Broker does not work. This is what my console output looks like after connecting to the WiFi-AP:

wifi connected...

 >>connected...

AT+S.STS=ip_ipaddr

AT-S.Var:ip_ipaddr=192.168.178.122

AT-S.OK

>>IP address is 192.168.178.122

AT+S.GCFG=nv_model

AT-S.Var:nv_model=SPWF04SA

AT-S.OK

>>model no is SPWF04SA

AT+S.MQTTCONN=mqtt.eclipse.org,1883,,,,,,,,,,

AT-S.ERROR:111:Request failed

+WIND:87:MQTT Closed:0:0

This is how I'm trying to connect the Broker:

char console_host[20];

char * hostname = "mqtt.eclipse.org";

uint32_t port_num = 1883;

memcpy(console_host, (const char*)hostname, strlen((char*)hostname));

wifi_mqtt_connect((uint8_t *)console_host, port_num);

Does anyone of you have an idea what I'm doing wrong?

Thanks for your help!

Fabian

    This topic has been closed for replies.