Skip to main content
Markus Burvall
Associate
Jan 29, 2018 12:55 PM UTC
Question

SPWF04S Factory Reset at power cycle

Posted on January 29, 2018 at 13:55

Hello,

We see a Factory Reset:1 When power cycling the SPWF04S. In about 80% of the times.

It is setup as a mini AP when the power cycle is done. Since the host is running lower UART speed than the SPWF04S it complicates things when the Factory default 115200 is used after Factory Reset.

AT-S.Var:build=170216-fd39c59-SPWF04S

AT-S.Var:fw_version=1.0.0

AT-S.Var:boot_version=1.0

+WIND:0:Console active

+WIND:3:Watchdog Running:20

+WIND:32:WiFi Hardware Started

+WIND:26:Started AP:GW_1002

+WIND:24:WiFi Up:0:192.168.0.50

+WIND:24:WiFi Up::fe80:0:0:0:280:e1ff:fec4:2d

+WIND:1:Poweron:170216-fd39c59-SPWF04S

+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:S

PWF04SA

+WIND:65:Factory Reset:1

+WIND:73:System Configuration Updated

+WIND:0:Console active

+WIND:3:Watchdog Running:20

+WIND:32:WiFi Hardware Started

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete:00

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete:00

#spwf04s #factory-reset
    This topic has been closed for replies.

    6 replies

    Markus Burvall
    Associate
    Jan 29, 2018 12:59 PM UTC
    Posted on January 29, 2018 at 13:59

    And the questions: :)

    Could the flash really be corrupted 80 % of the time?

    How is this behaviour avoided?

    Is it possible to change the factory settings? (Add new certificates, change speed, SSID etc.)

    Elio Cometti
    Visitor II
    Jan 29, 2018 10:04 PM UTC
    Posted on January 29, 2018 at 22:04

    Hello,

    the config section is updated during bootstrap and a checksum is written to allow the verification of section consistency.

    If a reset o power cycle is performed during this step then the config section will be partially updated and become inconsistent.

    Hence, a reset or power drop/cycle must be avoided within, let's say, 1 second from boot.

    The config factory setting is included in the FW at compile time and cannot be changed by AT command.

    As far as I know, TLS and WPA-E certificates are not erased by factory restore.

    Antonio Roman
    Associate
    Feb 14, 2018 12:48 PM UTC
    Posted on February 14, 2018 at 13:48

    Hi,

    I have a struggle with save the configuration into wifi module. The module lostd their configuration after a powerdown cycle, giving these messages:

    +WIND:65:Factory Reset:1

    +WIND:73:System Configuration Updated

    It occurrs ALWAYS, and is very rarelly that preserve the configuration after a powerdown and boot. I followed the sugested steps to avoid that problem, leaving a 2 seconds of gap time between saving the configuration and powerdown, but occurs always the same, factory reset.

    Are there some additonal advices to avoid this problem?

    Elio Cometti
    Visitor II
    Feb 20, 2018 3:38 PM UTC
    Posted on February 20, 2018 at 16:38

    My guess is that the wifi module is booted while the power line is not stable.

    Could you please verify there are not power drops during boot?

    Could you please also try keeping the module reset when the power is given to the module and check if the two indications above are still printed? (e.g. if you are using a X-NUCLEO-IDW04A1, keep pressed the reset button, connect the power and then release the reset button)

    Ivan Castillo
    Visitor II
    Apr 29, 2018 3:40 PM UTC
    Posted on April 29, 2018 at 17:40

    Hello,

    I have the same problem. I introduce the module in Station mode and when I power down the module and power up I recieve the '

    +WIND:65:Factory Reset:1'

    I have 200 circuits with the spwf01 and all was ok.

    I only have the problem with the spwf04.

    Someone can help me? I am 5 days working at this problem and I am desespersted.

    Best regards.

    florian239955_st
    Associate III
    May 1, 2018 7:11 AM UTC
    Posted on May 01, 2018 at 09:11

    Hi,

    as I mentioned in the SPWF01 to SPWF04 migration thread, this could be a power up / sequencing issue.

    After repowering, I always got a factory reset. I changed the the pull-up to a pull-down resistor at the reset line. Now I don't have this problem anymore.

    It looks like the timing of my 3.3V voltage and the reset line are not in the right sequence for the module...

    BR

    Flow