Skip to main content
florian239955_st
Associate III
Mar 2, 2018 3:34 PM UTC
Question

SPWF04: Need a pull down at RTS

Posted on March 02, 2018 at 16:34

Hi,

I changed on my hardware the SPWF01 against a SPWF04 module. I communicate with the module via a STM32. If I use the SPWF04 module, I need a pull down resistor at the SPWF RTS output to get the communication working. I wonder why? Any ideas?

BR,

Flow

    This topic has been closed for replies.

    2 replies

    Tia Meng
    Associate
    Apr 2, 2018 11:10 PM UTC
    Posted on April 03, 2018 at 01:10

    We have a customer using 

    SPWF04 recently and found this module when running at standby mode would draw around >1mA current rather than uA level mentioned in the datasheet. They were using SPWF01 before and did not see this problem. May I know if SPWF04 could be a compatible replacement for SPWF01, any notice/tips for Hardware redesign or AT comment settings? I have asked them to pull down some GPIO externally e.g. GPIO7,8,9, but standby current is mA.  Thanks. 

    Elio Cometti
    Visitor II
    Apr 4, 2018 9:26 AM UTC
    Posted on April 04, 2018 at 11:26

    Hello Flow,

    the SPWF RTS output is not driven when HW flow control is disabled (console_hwfc=0).

    Please verify the HW flow control is enabled on both SPWF and host micro, or HW flow control is disabled on both SPWF and host micro.

    Regards,

    Elio