Skip to main content
Mareike H
Associate II
Sep 15, 2017 2:50 PM UTC
Question

SPWF04 filesystem update via UART

Posted on September 15, 2017 at 16:50

Hi,

I am using the SPWF04 and want to update the filesystem via UART.

Is it possible?

For the SPWF01 there is the command AT+S.HTTPDFSWRITE but thats not working with the SPWF04.

I've read in another post that it might be possible with FLASHER/ST-LINK (wired UART/SWD) but I can't find any further informations.

Thanks for your help!

    This topic has been closed for replies.

    1 reply

    Elio Cometti
    Visitor II
    Sep 15, 2017 4:24 PM UTC
    Posted on September 15, 2017 at 18:24

    In the SPWF04 the filesystem is stored in the STM32's internal flash, hence you can use the STM32 Flash loader demonstrator (go to

    http://www.st.com

    and search for FLASHER-STM32 or STM32 Flash loader demonstrator).

    The starting address of the filesystem is:

    - 0x8100000 for Application Disk

    - 0x8110000 for User Disk