Skip to main content
gary239955_stm1_stmicro
Associate
Apr 25, 2015 5:20 AM UTC
Question

SPWF01XX Firmware Upgrade (usart)

Posted on April 25, 2015 at 07:20

Hello

I need to update the firmware (need the 1 command the is in release 3.3)for the above module. I have contacted the local ST agent and have received the required programs and files for the upgrade (via usart)

(SPWF01S Wi-Fi  documentation package W48 - FW3.3)

I run the FW_update.bat file and do what is required including (BOOT0 pin needs to be pulled high (3.3v))

I always get a 'Initial ACK not received from module'' response error. 

Question: I run the serial port just with Rx,Tx and Gnd. Do I need RTS and CTS? 

Please note my serial comms can communicate with the module normally.  
    This topic has been closed for replies.

    2 replies

    Gerardo GALLUCCI
    ST Employee
    Apr 26, 2015 9:56 AM UTC
    Posted on April 26, 2015 at 11:56

    Hi Gary,

    usually, when I see that error, means I did not provide module a reset AFTER boot pin has been pulled high.

    Tx+Rx+GND are enough. Do not forget to provide 3V3 to module :)

    Let me know.

    jerry

    ps: if you are moving to FW3.3, I really suggest you to move directly fo FW3.4.

    gary239955_stm1_stmicro
    Associate
    May 27, 2015 9:23 PM UTC
    Posted on May 27, 2015 at 23:23

    Jerry

    I sorted a day after you posted this.

    I had a corrupt software download. 

    Thanks for the help.