Skip to main content
toby
Associate II
Nov 17, 2015 2:05 PM UTC
Question

SPWF01SA PCB Footprint

Posted on November 17, 2015 at 15:05

Between the rev 4 & Rev 6 datasheets there seems to have been a change in the centre pad size on the recommended footprint.  It now seems to ask for 8mm max x6mm max - previously it was specified as 10mmx8mm!  I have based all my designs on the larger pad.

The datasheet revision history does not seem to mention this change.  When did it come in? Has there been a revison change on the module?

#spwf01sa
    This topic has been closed for replies.

    3 replies

    Gerardo GALLUCCI
    ST Employee
    Nov 17, 2015 2:43 PM UTC
    Posted on November 17, 2015 at 15:43

    Hi Toby,

    changes took place in Rev5.

    Module's HW did not change. I mean, there was only a mismatch on picture number 7. Pad size was (and is still) 8x6mm.

    Normally solder paste takes 80% of pad layout. You can reduce this percentage to 60%.

    Regards

    jerry

    toby
    tobyAuthor
    Associate II
    Nov 17, 2015 2:53 PM UTC
    Posted on November 17, 2015 at 15:53

    Ok thanks for the info.  I will have to update my footprint to match for the next production boards. 

    Unfortunately then I assume that then there is potentially a risk of shorts then with the larger pad and our current production assemblies?

    Gerardo GALLUCCI
    ST Employee
    Nov 17, 2015 3:03 PM UTC
    Posted on November 17, 2015 at 16:03

    Within 60% there are no risks, because of solder resist (vias are ok)