Skip to main content
pietro
Associate
Feb 25, 2015 11:08 AM UTC
Question

SPWF01SA IBSS

Posted on February 25, 2015 at 12:08

Hi, I'm using STEVAL-IDW001V1 and STEVAL-PCC018V1 boards.

I set up wifi into IBSS mode named ''ADHOC'' but I cannot detect it from the telephone or browser.

I've the impression I'm not creating the ADHOC network. Where's the issue?

I'm attaching data. 

+WIND:2:Reset

+WIND:1:Poweron (141106-0950875-SPWF01S)

+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc.  All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

+WIND:19:WiFi Join:16:BD:EC:00:B3:C5

+WIND:25:WiFi Association with 'ADHOC' successful

+WIND:51:WiFi Handshake Complete

+WIND:24:WiFi Up:192.168.1.101

# Status & Statistics:

#  version = 141106-0950875-SPWF01S 

#  reset_reason = 2

#  conf_flag = 5

#  system_uptime = 103

#  system_sleeptime = 0

#  gpio_enable = 0

#  captiveportal = 0

#  wifi_state = 10

#  wifi_bssid = 16:BD:EC:00:B3:C5

#  wifi_aid = 0

#  wifi_channelnum = 6

#  wifi_sup_rate_mask = 0x003FFFCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_chan_activity2 = 0x00000020

#  wifi_max_tx_power = 18

#  wifi_reg_country = 

#  wifi_dtim_period = 0

#  wifi_sleeping = 1

#  wifi_num_assoc = 0

#  ip_ipaddr = 192.168.1.101

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.1.1

#  ip_dns = 208.67.222.222

#  ip_sock_open = 0

#  ip_sockd_port = 0

#  free_heap = 21656

#  min_heap = 20312

#  current_time = 2342

OK

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01SA1

#  nv_serial = 4313D25167

#  nv_wifi_macaddr = 00:80:E1:FF:BA:C7

#  blink_led = 0

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 115200

#  console1_hwfc = 0

#  console1_enabled = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 41:44:48:4F:43:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 5

#  wifi_channelnum = 6

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 2

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 0

#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 00:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wpa_psk_text = 

#  ip_use_dhcp = 0

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-FF-BA-C7

#  ip_apdomainname = captiveportal.net

#  ip_ipaddr = 192.168.1.101

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.1.1

#  ip_dns = 192.168.1.1

#  ip_http_get_recv_timeout = 3000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

OK
    This topic has been closed for replies.

    4 replies

    danielkorbes
    Associate
    Feb 25, 2015 4:56 PM UTC
    Posted on February 25, 2015 at 17:56

    Pietro, I had the same problem.

    To solve it I need to update the module. Try v3.3.

    And update it OTA. Using UART I ''brick'' the module...

    Gerardo GALLUCCI
    ST Employee
    Feb 26, 2015 7:48 AM UTC
    Posted on February 26, 2015 at 08:48

    IBSS was included into FW 20140805, namely FW3.2

    Gerardo GALLUCCI
    ST Employee
    Feb 26, 2015 9:08 AM UTC
    Posted on February 26, 2015 at 10:08

    Did you set a static IP address also on smartphone?

    Depending on OS, this step is mandatory.

    This step is not needed, for example, using iOS.
    pietro
    pietroAuthor
    Associate
    Feb 26, 2015 10:27 AM UTC
    Posted on February 26, 2015 at 11:27

    Ok, thanks, understood. It works.

    Thank you Gerardo!

    Bye