Skip to main content
Roma Jam
Associate
Nov 19, 2014 1:43 PM UTC
Question

SPWF01SA HTTP Request

Posted on November 19, 2014 at 14:43

Hello everybody!

It is interesting to me to make an electronic device which can receive data from the mobile devices (e.g. Mobile Phone or Computer). The main idea is to send data to electronic device by using the html web page and internal browser of the mobile device. So I bought module SPWF01SA.

Using the reference manual to the SPWF module I understood that it can working in two modes which is interesting to me. Either the Mini AP mode or a IBSS mode.

In the IBSS mode i can use the HTML web pages was writed in internal memory (like an output_demo.html) and to send the string to my SPWF module and get it by the UART port. Yes I done it.

But my question is next.

Is there any ways to get raw HTTP request from the client to my server (either in IBSS mode or miniAP mode) by the UART (or SPI)?

Hope, somebody can help me or say smth interesting about this. 

Grazie!

#spwf01sa #wifi
    This topic has been closed for replies.

    11 replies

    Gerardo GALLUCCI
    ST Employee
    Nov 22, 2014 6:12 PM UTC
    Posted on November 22, 2014 at 19:12

    With ''messages'' I mean bytes which are sent over UART to the SPWF when it's in DataMode.

    Let me know if you are in trouble with socket server Command/Data mode.

    j