Skip to main content
sergetr
Associate
Feb 23, 2017 9:04 PM UTC
Question

SPWF01SA Do not list open networks

Posted on February 23, 2017 at 22:04

Hello I'm using SPWF01SA wifi module. When I do AT+S.SCAN all the available networks around are listed except the open ones. I can see every password protected networks (WPA2) but the open networks are not even seen by the module. Is there any way to list and connect to a non password protected network? Thank you very much.

    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Feb 24, 2017 1:05 PM UTC
    Posted on February 24, 2017 at 14:05

    Hi Serge,

    I see every kind of protection:

    ...

    wpa-psk > 3: BSS 02:62:1F:51:8F:0B CHAN: 01 RSSI: -53 SSID: 'IoT' CAPS: 0411 WPA2 WPS

    wep > 4: BSS 02:62:1F:51:8F:08 CHAN: 01 RSSI: -54 SSID: 'IoT_W' CAPS: 0011

    wpa-e 5: BSS 02:62:1F:51:8F:09 CHAN: 01 RSSI: -54 SSID: 'IoT_E' CAPS: 0011 WPA2

    open > 6: BSS B8:62:1F:51:8F:0A CHAN: 01 RSSI: -53 SSID: 'IoT_O' CAPS: 0001 WPS

    Are you sure AP is broadcasting its SSID? If not, set wifi_region to an higher value than 1, according to your Country rules.