Skip to main content
cbertrand
Associate
Dec 17, 2014 9:35 AM UTC
Question

SPWF01S Station connection problems

Posted on December 17, 2014 at 10:35

Hi all,

I'm using the WiFi module to connect to infra WiFi in socket server mode.

The module return (through serial link) that connection to WiFi is OK.

But sometimes, in the WiFi router interface (a Freebox), the module is seen but stay in a not reachable status. At the end, it's not possible to send data to socket server. Even a ping to module address doesn't work.

Sometimes it works perfectly... for few hours and then back to unreachable.

SPWF01S output on startup :

+WIND:1:Poweron (141106-0950875-SPWF01S)

 

+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc.  All rights Reserved.

 

+WIND:3:Watchdog Running

 

+WIND:0:Console active

 

+WIND:32:WiFi Hardware Started

 

+WIND:19:WiFi Join:F4:CA:E5:D3:65:34

 

+WIND:25:WiFi Association with 'freebox_EVB' successful

 

+WIND:51:WPA Handshake Complete

 

+WIND:24:WiFi Up:192.168.1.43

 

OK

 

The OK at the end is the answer of socket server start command :

AT+S.SOCKD=27024

My config config is :

# Dumping All Configuration Keys:

 

#  nv_manuf = ST

 

#  nv_model = SPWF01SA1

 

#  nv_serial = 4313D07237

 

#  nv_wifi_macaddr = 00:80:E1:FF:B5:14

 

#  blink_led = 0

 

#  wind_off_low = 0x00200000

 

#  wind_off_medium = 0x00000008

 

#  wind_off_high = 0x00000000

 

#  user_desc = IoTMesh

 

#  escape_seq = at+s.

 

#  localecho1 = 0

 

#  console1_speed = 115200

 

#  console1_hwfc = 0

 

#  console1_enabled = 1

 

#  sleep_enabled = 0

 

#  standby_enabled = 0

 

#  standby_time = 10

 

#  wifi_tx_msdu_lifetime = 0

 

#  wifi_rx_msdu_lifetime = 0

 

#  wifi_operational_mode = 0x00000011

 

#  wifi_beacon_wakeup = 1

 

#  wifi_beacon_interval = 100

 

#  wifi_listen_interval = 0

 

#  wifi_rts_threshold = 3000

 

#  wifi_ssid = 66:72:65:65:62:6F:78:5F:45:56:42:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

#  wifi_ssid_len = 11

 

#  wifi_channelnum = 6

 

#  wifi_opr_rate_mask = 0x00003FCF

 

#  wifi_bas_rate_mask = 0x0000000F

 

#  wifi_mode = 1

 

#  wifi_auth_type = 0

 

#  wifi_atim_window = 0

 

#  wifi_powersave = 0

 

#  wifi_tx_power = 18

 

#  wifi_rssi_thresh = 0

 

#  wifi_rssi_hyst = 0

 

#  wifi_ap_idle_timeout = 120

 

#  wifi_beacon_loss_thresh = 10

 

#  wifi_priv_mode = 2

 

#  wifi_wep_keys[0] = 49:6F:54:4D:65:73:68:30:30:38:30:45:31:00:00:00

 

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

#  wifi_wep_key_lens = 0D:00:00:00

 

#  wifi_wep_default_key = 0

 

#  wifi_wpa_psk_raw = XXX...

 

#  wifi_wpa_psk_text = XXX...

 

#  ip_use_dhcp = 0

 

#  ip_use_httpd = 1

 

#  ip_mtu = 1500

 

#  ip_hostname = GWM4_0080E1

 

#  ip_apdomainname = gwm4_iotmesh.net

 

#  ip_ipaddr = 192.168.1.51

 

#  ip_netmask = 255.255.255.0

 

#  ip_gw = 192.168.1.254

 

#  ip_dns = 192.168.1.254

 

#  ip_http_get_recv_timeout = 3000

 

#  ip_dhcp_timeout = 20

 

#  ip_sockd_timeout = 250

 

 

OK

 

I really don't understand why module is sometimes reachable and sometimes not.

Any ideas ?

Thanks.
    This topic has been closed for replies.

    16 replies

    cbertrand
    cbertrandAuthor
    Associate
    Dec 22, 2014 2:00 PM UTC
    Posted on December 22, 2014 at 15:00

    New information,

    I changed my WiFi router security to WPA2-PSK AES.

    Now, the connection always succeed !!

    There is something really strange arround security setting.

    akravchenko9
    Associate
    Jan 4, 2015 9:14 PM UTC
    Posted on January 04, 2015 at 22:14

    Same problems...

    Everything is fine until I did not use SoftPerfect Network Scanner (https://www.softperfect.com/). After using this software -- WiFi module is down from outside. I can ping my PC ( from the WiFi module), but I can not open WiFi module web page, I can not ping the WiFi module from the PC and so on...

    https://www.softperfect.com/products/networkscanner/

    Also could you please check DNS variable in case when WiFi module is working without DHCP (at+s.scfg=ip_use_dhcp,0) See post #3
    Gerardo GALLUCCI
    ST Employee
    Jan 7, 2015 10:20 AM UTC
    Posted on January 07, 2015 at 11:20

    Hi Artem,

    if module is working without DHCP, you have to set IP, netmask, gateway and DNS addresses (by at+s.scfg command).

    If DNS is not set, then Resolver1 of OpenDNS is used (http://en.wikipedia.org/wiki/OpenDNS)

    j

    akravchenko9
    Associate
    Jan 7, 2015 10:39 AM UTC
    Posted on January 07, 2015 at 11:39

    I did it.

    Compare with topic-starter, situation is similar in my case

    You can look at post #1 and #3. IP, netmask, gateway and DNS was set, but after module boot and using AT command ( AT+S.STS ) I see that DNS address is different.

    Gerardo GALLUCCI
    ST Employee
    Jan 7, 2015 1:25 PM UTC
    Posted on January 07, 2015 at 14:25

    So, you did:

    - at+s.scfg=ip_use_dhcp,0

    - at+s.scfg=ip_ipaddr,A1

    - at+s.scfg=ip_netmask,A2

    - at+s.scfg=ip_gw,A3

    - at+s.scfg=ip_dns,A4

    - at&w

    - at+cfun=1

    ...and after reboot, and wifi up message indication, you see:

    - ''at+s.sts=ip_dns'' different from A4? openDNS address there?

    akravchenko9
    Associate
    Jan 7, 2015 2:11 PM UTC
    Posted on January 07, 2015 at 15:11

    ============================

    = Start module with DHCP

    ============================

    at+cfun=1

    +WIND:2:Reset

    +WIND:1:Poweron (140805-3f58d6b-SPWF01S)

    +WIND:13:ST SPWF01SA IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.

    +WIND:3:Watchdog Running

    +WIND:0:Console active

    +WIND:32:WiFi Hardware Started

    +WIND:21:WiFi Scanning

    +WIND:35:WiFi Scan Complete (0x0)

    +WIND:19:WiFi Join:6C:62:6D:24:99:4D

    +WIND:25:WiFi Association with 'Unknow' successful

    +WIND:51:WPA Handshake Complete

    +WIND:24:WiFi Up:192.168.1.126

    at&v

    # Dumping All Configuration Keys:

    # nv_manuf = ST

    # nv_model = SPWF01SA

    # nv_serial = 1613D28033

    # nv_wifi_macaddr = 00:80:E1:FF:8D:10

    # blink_led = 0

    # wind_off_low = 0x00000000

    # wind_off_medium = 0x00000000

    # wind_off_high = 0x00000000

    # user_desc = anonymous

    # escape_seq = at+s.

    # localecho1 = 1

    # console1_speed = 115200

    # console1_hwfc = 0

    # console1_enabled = 1

    # sleep_enabled = 0

    # standby_enabled = 0

    # standby_time = 10

    # wifi_tx_msdu_lifetime = 0

    # wifi_rx_msdu_lifetime = 0

    # wifi_operational_mode = 0x00000011

    # wifi_beacon_wakeup = 1

    # wifi_beacon_interval = 100

    # wifi_listen_interval = 0

    # wifi_rts_threshold = 3000

    # wifi_ssid = 55:6E:6B:6E:6F:77:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_ssid_len = 6

    # wifi_channelnum = 6

    # wifi_opr_rate_mask = 0x00003FCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_mode = 1

    # wifi_auth_type = 0

    # wifi_atim_window = 0

    # wifi_powersave = 0

    # wifi_tx_power = 18

    # wifi_rssi_thresh = 0

    # wifi_rssi_hyst = 0

    # wifi_ap_idle_timeout = 120

    # wifi_beacon_loss_thresh = 10

    # wifi_priv_mode = 2

    # wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_key_lens = 00:00:00:00

    # wifi_wep_default_key = 0

    # wifi_wpa_psk_raw = 37:50:6B:84:D3:87:77:7D:24:6E:04:9F:86:AD:AB:65:FB:53:4B:1F:81:4D:A9:49:9C:C3:BA:B5:96:89:FD:D5

    # wifi_wpa_psk_text = Gogo

    # ip_use_dhcp = 1

    # ip_use_httpd = 1

    # ip_mtu = 1500

    # ip_hostname = iwm-FF-8D-10

    # ip_apdomainname = captiveportal.net

    # ip_ipaddr = 192.168.1.8

    # ip_netmask = 255.255.255.0

    # ip_gw = 192.168.1.3

    # ip_dns = 192.168.1.3

    # ip_http_get_recv_timeout = 3000

    # ip_dhcp_timeout = 20

    OK

    at+s.sts

    # Status & Statistics:

    # version = 140805-3f58d6b-SPWF01S

    # reset_reason = 2

    # conf_flag = 5

    # system_uptime = 13

    # system_sleeptime = 0

    # gpio_enable = 0

    # captiveportal = 0

    # wifi_state = 10

    # wifi_bssid = 6C:62:6D:24:99:4D

    # wifi_aid = 2

    # wifi_channelnum = 10

    # wifi_sup_rate_mask = 0x003FFFCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_chan_activity2 = 0x00003FFF

    # wifi_max_tx_power = 18

    # wifi_reg_country = GB

    # wifi_dtim_period = 2

    # wifi_sleeping = 1

    # wifi_num_assoc = 0

    # ip_ipaddr = 192.168.1.126

    # ip_netmask = 255.255.255.0

    # ip_gw = 192.168.1.3

    # ip_dns = 192.168.1.3

    # ip_sock_open = 0

    # ip_sockd_port = 0

    # free_heap = 24336

    # min_heap = 24192

    # current_time = 359

    ====================

    =  at+s.scfg=ip_use_dhcp,0

    ====================

    OK

    at+s.scfg=ip_use_dhcp,0

    OK

    at&w

    ===========

    = Start module without DHCP

    ===========

    OK

    at+cfun=1

    +WIND:2:Reset

    +WIND:1:Poweron (140805-3f58d6b-SPWF01S)

    +WIND:13:ST SPWF01SA IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.

    +WIND:3:Watchdog Running

    +WIND:0:Console active

    +WIND:32:WiFi Hardware Started

    +WIND:21:WiFi Scanning

    +WIND:35:WiFi Scan Complete (0x0)

    +WIND:19:WiFi Join:6C:62:6D:24:99:4D

    +WIND:25:WiFi Association with 'Unknow' successful

    +WIND:51:WPA Handshake Complete

    +WIND:24:WiFi Up:192.168.1.8

    at+s.sts

    # Status & Statistics:

    # version = 140805-3f58d6b-SPWF01S

    # reset_reason = 2

    # conf_flag = 5

    # system_uptime = 9

    # system_sleeptime = 0

    # gpio_enable = 0

    # captiveportal = 0

    # wifi_state = 10

    # wifi_bssid = 6C:62:6D:24:99:4D

    # wifi_aid = 2

    # wifi_channelnum = 10

    # wifi_sup_rate_mask = 0x003FFFCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_chan_activity2 = 0x00003FFF

    # wifi_max_tx_power = 18

    # wifi_reg_country = GB

    # wifi_dtim_period = 2

    # wifi_sleeping = 1

    # wifi_num_assoc = 0

    # ip_ipaddr = 192.168.1.8

    # ip_netmask = 255.255.255.0

    # ip_gw = 192.168.1.3

    # ip_dns = 208.67.222.222

    # ip_sock_open = 0

    # ip_sockd_port = 0

    # free_heap = 24384

    # min_heap = 24240

    # current_time = 107

    OK

    at&v

    # Dumping All Configuration Keys:

    # nv_manuf = ST

    # nv_model = SPWF01SA

    # nv_serial = 1613D28033

    # nv_wifi_macaddr = 00:80:E1:FF:8D:10

    # blink_led = 0

    # wind_off_low = 0x00000000

    # wind_off_medium = 0x00000000

    # wind_off_high = 0x00000000

    # user_desc = anonymous

    # escape_seq = at+s.

    # localecho1 = 1

    # console1_speed = 115200

    # console1_hwfc = 0

    # console1_enabled = 1

    # sleep_enabled = 0

    # standby_enabled = 0

    # standby_time = 10

    # wifi_tx_msdu_lifetime = 0

    # wifi_rx_msdu_lifetime = 0

    # wifi_operational_mode = 0x00000011

    # wifi_beacon_wakeup = 1

    # wifi_beacon_interval = 100

    # wifi_listen_interval = 0

    # wifi_rts_threshold = 3000

    # wifi_ssid = 55:6E:6B:6E:6F:77:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_ssid_len = 6

    # wifi_channelnum = 6

    # wifi_opr_rate_mask = 0x00003FCF

    # wifi_bas_rate_mask = 0x0000000F

    # wifi_mode = 1

    # wifi_auth_type = 0

    # wifi_atim_window = 0

    # wifi_powersave = 0

    # wifi_tx_power = 18

    # wifi_rssi_thresh = 0

    # wifi_rssi_hyst = 0

    # wifi_ap_idle_timeout = 120

    # wifi_beacon_loss_thresh = 10

    # wifi_priv_mode = 2

    # wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

    # wifi_wep_key_lens = 00:00:00:00

    # wifi_wep_default_key = 0

    # wifi_wpa_psk_raw = 37:50:6B:84:D3:87:77:7D:24:6E:04:9F:86:AD:AB:65:FB:53:4B:1F:81:4D:A9:49:9C:C3:BA:B5:96:89:FD:D5

    # wifi_wpa_psk_text = Gogo

    # ip_use_dhcp = 0

    # ip_use_httpd = 1

    # ip_mtu = 1500

    # ip_hostname = iwm-FF-8D-10

    # ip_apdomainname = captiveportal.net

    # ip_ipaddr = 192.168.1.8

    # ip_netmask = 255.255.255.0

    # ip_gw = 192.168.1.3

    # ip_dns = 192.168.1.3

    # ip_http_get_recv_timeout = 3000

    # ip_dhcp_timeout = 20

    OK