Skip to main content
egoltzman
Senior
Sep 11, 2017 7:03 AM UTC
Question

SPWF01 - Why wifi_init restore module to factory default (AT+&F)

Posted on September 11, 2017 at 09:03

I'm using STM32 WiFi Cube Extension 3.02 and I see that calling wifi_init restore my module to factory default.

I want the latest AP setup to be saved between module power cycles, if one was set, and by calling wifi init I remove this setup every time the module is started.

I can of course comment it out but I was wondering why it is there from the first place, maybe I'm doing something wrong?

Thanks,

Eyal 

#spwf01
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    Sep 12, 2017 10:31 PM UTC
    Posted on September 13, 2017 at 00:31

    Probably because it makes supporting the demo easier. ie a million questions about it not working after configuring it to do X

    With modems ATZ is frequently used to load the settings saved with AT&W

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..