Skip to main content
florian239955_st
Associate III
Dec 19, 2016 1:48 PM UTC
Solved

SPWF01: Save network settings after firmware upgrade?

Posted on December 19, 2016 at 14:48

Hi Jerry,

is it possible to save the network connection settings (SSID name, password, etc.), that after a firmware update of the SPWF01the settings are still avaliable and the module connects again to the network?

In older firmware upates, I have to setup the module with the network settings again after a firmware update.

Cheers,

Flow 

#firmare-update #spwf01
    This topic has been closed for replies.
    Gerardo GALLUCCI
    Gerardo GALLUCCIBest answer
    ST Employee
    Dec 19, 2016 5:20 PM UTC
    Posted on December 19, 2016 at 18:20

    Hi Flow,

    usually a FW update reloads factory setting if configuration variables have been changed. In this case, a specific WIND appears on console (WIND:73).

    If configuration variables are not moved/changed/etc from different FW versions, than WIND:73 will not appear on console, and user variables are not lost.

    Hope it clarifies

    jerry

    2 replies

    Gerardo GALLUCCI
    Gerardo GALLUCCIBest answer
    ST Employee
    Dec 19, 2016 5:20 PM UTC
    Posted on December 19, 2016 at 18:20

    Hi Flow,

    usually a FW update reloads factory setting if configuration variables have been changed. In this case, a specific WIND appears on console (WIND:73).

    If configuration variables are not moved/changed/etc from different FW versions, than WIND:73 will not appear on console, and user variables are not lost.

    Hope it clarifies

    jerry

    florian239955_st
    Associate III
    Dec 21, 2016 10:00 AM UTC
    Posted on December 21, 2016 at 11:00

    Hi Jerry,

    thanks for explaining.

    So, I will save the network settings before I update the module...

    Cheers,

    Flow