Skip to main content
Sylvain Basset
Associate
Feb 18, 2018 5:35 PM UTC
Solved

SPWF01: Running example applications

Posted on February 18, 2018 at 18:35

Hi,

I get troubles to start with my new IDW01M1 module.

I use it with the NUCLEO-L053R8 board, but none of applications provided with the WiFi CubeExpansion package works with my hardware.

For example, I load the 'WiFi_VCOM' application to the main board. The application launches, but it cannot set the connection with WiFi module at start (message 'Error in baud-rate auto-detection...' on termnial).

Again, with the 'Client_socket' application: it starts, ask for identifiers, and freeze at WiFi module initialization.

It seems that there are no communications at all with the module.

I tried Resets on both boards, and Factory setting reset on WiFi module (set GPIO0 high at start), without success.

Jumpers are placed on JP3 and JP4, no jumpers on JP1/JP2

LED1 is on, LED2, LED3, LED4 are off.

Does I missed something obvious, or my hardware is broken ???

#x-cube-wifi #spwf01
    This topic has been closed for replies.
    Sylvain Basset
    Sylvain BassetBest answer
    Associate
    Mar 3, 2018 1:23 PM UTC
    Posted on March 03, 2018 at 13:23

    I found that the problem comes from side effect between sysctick and UART interrupt.

    The Systick interrupt calls Process_WiFi() function (wifi_module.c). At begining, interruptions are disabled during  pop_buffer_queue() call (wifi_module.c, line 1093). So UART reception is disabled during this time.

    It seems that this critical section last too long compared to UART IRQ frequency. I found that memset() operation, used to initialize the poping buffer, takes too much time.

    So, I silly reduced the size of buffer initialization (ring_buffer.c, line 188) :

          memset(pop_buffer, 0x00 , MAX_BUFFER_GLOBAL); --> to : memset(pop_buffer, 0x00 , ELEMENT_SIZE); 

    And it works !!!  I'm now able to connect to my AP and open socket.

    Just note that this is a dirty workaround. I just tested a connection to AP . I dont know what happens when 'data chunk' is enabled.

    I see this forum is not very active but i hope this will help someone who google it.

    2 replies

    Sylvain Basset
    Associate
    Feb 23, 2018 12:33 PM UTC
    Posted on February 23, 2018 at 13:33

    Hi,

    I did further investigations and it appears that my example applications stucks in infinite loop at wifi module initialization :

    In wifi_module.c:

    while(IO_status_flag.WiFi_WIND_State.WiFiHWStarted != WIFI_TRUE)

    {

    __NOP(); //nothing to do

    }

    I found these threads

    https://community.st.com/0D50X00009XkgFFSAZ

    and

    https://community.st.com/0D50X00009XkXvmSAF

    describing the same problem.

    So, I looked at ring_buffer content after wifi module reset, and I got WIND strings with some missing character :

    ie:

    \r\n+WND:1:peron ...

    In the second thread I mention, it said that missing characters means 'issue on uart management' (

    see Gerardo Gallucci post on May 2, 2017 10:20 AM)

    But it remains unclear how to fix that problem. I tried to switch Timer and Uart IRQ priority but it has no effect.

    Can you help me to resolve this.

    Regards

    Sylvain Basset

    PS: my first port contains a mistake : LED 4 (orange) in ON on my module

    Sylvain Basset
    Sylvain BassetAuthorBest answer
    Associate
    Mar 3, 2018 1:23 PM UTC
    Posted on March 03, 2018 at 13:23

    I found that the problem comes from side effect between sysctick and UART interrupt.

    The Systick interrupt calls Process_WiFi() function (wifi_module.c). At begining, interruptions are disabled during  pop_buffer_queue() call (wifi_module.c, line 1093). So UART reception is disabled during this time.

    It seems that this critical section last too long compared to UART IRQ frequency. I found that memset() operation, used to initialize the poping buffer, takes too much time.

    So, I silly reduced the size of buffer initialization (ring_buffer.c, line 188) :

          memset(pop_buffer, 0x00 , MAX_BUFFER_GLOBAL); --> to : memset(pop_buffer, 0x00 , ELEMENT_SIZE); 

    And it works !!!  I'm now able to connect to my AP and open socket.

    Just note that this is a dirty workaround. I just tested a connection to AP . I dont know what happens when 'data chunk' is enabled.

    I see this forum is not very active but i hope this will help someone who google it.