Skip to main content
be_it
Associate II
Jun 4, 2018 8:07 AM UTC
Question

SPWF01 NRND alternative

Posted on June 04, 2018 at 10:07

Hello,

We are using SPWF01SA.11 to provide WIFI connectivity to our items that become micro-webservers.

Our provider told us that the product entered in NRND (Not Recommended for New Design) phase.

Will ST provide an equivalent/alternative or does this kind of WIFI solution become totally obsolete ?

Thank you for the answer.

Regards.

Vincent

    This topic has been closed for replies.

    5 replies

    florian239955_st
    Associate III
    Jun 4, 2018 8:46 AM UTC
    florian239955_st
    Associate III
    Jun 4, 2018 11:06 AM UTC
    Posted on June 04, 2018 at 11:06

    Ohh... SPWF04 is now also NRND

    be_it
    be_itAuthor
    Associate II
    Jun 5, 2018 8:21 AM UTC
    Posted on June 05, 2018 at 10:21

    Thank you Flow for the answer and bitter finding.

    So it seems to be the end of SPWF0x story.

    Now we have until Dec 2018 as LTB (Last Time Buy).

    Does anyone has a solution for (easy) replacement of these pratical Wifi modules

    with UART and integrated webserver ?

    florian239955_st
    Associate III
    Jun 5, 2018 10:34 AM UTC
    Posted on June 05, 2018 at 10:34

    It's so bitter: End of last year I did a re-design and switched from SPWF01 to SPWF04 to be future-proof. And now the SPWF04 is obsolete, too...

    I will probably switch back to Microchip

    https://www.microchip.com/wwwproducts/en/ATWINC1500

     
    be_it
    be_itAuthor
    Associate II
    Jun 13, 2018 3:16 PM UTC
    Posted on June 13, 2018 at 17:16

    Is there an existing ST module that could give the same features as SPWF01SA.11 with Ethernet instead Wifi ?

    Our needs are :

    - AT Command to set network parameters  from UART

    - AT Command to write Html files to the module from UART

    - output.cgi command to send Text from webserver client to UART

    We could then replace our Uart to Wifi webserver by a compatible UART to Ethernet webserver.

    That would need an ethernet cable instead of wifi but our customers could deal with such a solution.