Skip to main content
Rohan Gupta
Visitor II
Jan 13, 2018 2:07 PM UTC
Question

SPW40SA Certificate Error:23

Posted on January 13, 2018 at 15:07

Hello Everyone,

Even if I load the DER binary format into my wifi-module SPW40SA , The subject key identifier won't be detected automatically by the module. I have to manually add the key and if I try the simple AT+S.HTTPGET demostrated in AN4963 document for the 

http://www.amazon.com

 i get Certificate error:23(The CA could not be found)  . I even tried with the PEM format also but still the same error exists . 

Does anyone have the same problem or any hint on how to resolve this issue ? 

#wifi #certificate #spwf40sa #tlscert
    This topic has been closed for replies.

    1 reply

    Elio Cometti
    Visitor II
    Jan 18, 2018 9:43 AM UTC
    Posted on January 18, 2018 at 10:43

    Hello Rohan,

    Below you can find the log I get with my SPWF04SA module.

    Few guesses:

    - about the SubjectKeyId is not automatically extracted when loading DER certificate, maybe the certificate was not properly saved/converted. I downloaded the Root CA (VeriSignClass3PublicPrimaryCertificationAuthority-G5 from my location) certificate in PEM format and then I converted it to DER by:

    openssl x509 -in VeriSignClass3PublicPrimaryCertificationAuthority-G5.crt -out VeriSignClass3PublicPrimaryCertificationAuthority-G5.der -outform DER

    - about Certificate error:23, it may be a direct consequence of previous point, or maybe the certificate is incorrect or the auth field is incorrect.

    Following my log:

    AT+S.TLSCERT=ca,1239

    AT-S.SubjectKeyId:7F:D3:65:A7:C2:DD:EC:BB:F0:30:09:F3:43:39:FA:02:AF:33:31:33

    AT-S.OK

    AT+S.HTTPGET=www.amazon.com,,443,2,,,,

    AT-S.Skip CA

    AT-S.Loading:1:2

    AT-S.Http Server Status Code:200

    78b7

    <!doctype html><html class='a-no-js' data-19ax5a9jf='dingo'><!-- sp:feature:head-start -->

    (**** about 300KB of data ****)

    <!-- _

    .__(.)< (MEOW)

    \___)

    ~~~~~~~~~~~~~~~~~~-->

    <!-- sp:eh:yjfKwX939PaydD937gOR9o3LB3mpKMX5Sldv61bcWVPrzj1wR2lzfIAipZeinV8Erkffbg21v/Cfi0w03qcrJmfDdp4K8NlKoQwrlc4CajkTVTTJE500qA== -->

    AT-S.OK