Skip to main content
yoann LBY
Senior
Apr 3, 2018 2:27 PM UTC
Question

SPW04Sx Handshake certificate isue

Posted on April 03, 2018 at 16:27

hi,

SPWF047Sx, mode AP, FW1.1.0

CA, cert, key loading with AT+STLSCERT + datetime

cert 2x ecc bundle (prime256V1)

client connect to the wifi open.

next is AT+S.HTTPGET=192.168.0.2,conf,45061,2,,,config.txt,

AT-S.Skip CA

AT-S.Skip CA

AT-S.Loading:1:2

AT-S.Loading:2:2

AT-S.Loading:3:2

AT-S.Http Client Error:2

On the client (server https node js), i have bad signature and if i check AN4963 the problem is during decoding the CertificateVerify message: 

If the client has sent a digital certificate to the server, the client sends a

CertificateVerify

message signed with the client's private key. By verifying the signature of this message, the server can explicitly verify the ownership of the client digital certificate.

the size of signature sent by server to client (serverKeyexchange) is 71 bytes.

the size of signature sent by client to server (

CertificateVerify) is 70 bytes.

Is it the problem?

(if i use other client (curl) to do same test with same certificate, it works and size of signature for message

CertificateVerify

 is 71 bytes)

Help!

Thanks

Yoann

    This topic has been closed for replies.

    2 replies

    yoann LBY
    yoann LBYAuthor
    Senior
    Apr 4, 2018 4:50 PM UTC
    Posted on April 04, 2018 at 18:50

    hi,

    you continu investigation but have same problem. we replaced server by openssl (server reference) and the result is the same 'bad signature' during

    CertificateVerify

    .

    Signature Algorithm used is:

    TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256 .

    a help will be appriciate.

    thks

    Yoann

    Elio Cometti
    Visitor II
    Apr 4, 2018 7:52 PM UTC
    Posted on April 04, 2018 at 19:52

    Hello Yoann,

    I have just made a connection using a set of keys and certificates generated by me, from SPWF04 to an openssl server. The TLS handshake succeed but the HTTP GET fails because no answer is received to the HTTP request.

    The SPWF04 is AP with WPA encryption, the openssl server is forced to use ECDHE-ECDSA-AES128-GCM-SHA256 cipher.

    AT+S.HTTPGET=1.112,conf,4433,2,,,config.txt,

    AT-S.Loading:1:2

    AT-S.Loading:2:2

    AT-S.Loading:3:2

    AT-S.Http Client Error:4

    AT-S.ERROR:111:Request failed

    I'm attaching the openssl log. Could you please compare the certificate (dumped in the log) with your in order to highlight sensible differences?

    Regards,

    Elio

    ________________

    Attachments :

    openssl.log.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxqB&d=%2Fa%2F0X0000000b1F%2FohPmrFpOjVlRa6vE4PJt92E7hf_MvYbojZSphZDuB48&asPdf=false