Skip to main content
saurabh_7171
Visitor II
Oct 8, 2014 1:52 PM UTC
Question

Spirit1 transistion time between different modes using 48 Mhz Xtal

Posted on October 08, 2014 at 15:52

Hello Developers

In document “Spirit1_presentation_ST_Days.pdf“ and “Spirit1_datasheet.pdf�? transition time between different states /operating modes are calculated using 26 MHz and 52 MHz Xtal. So, please inform me how I can calculate these values for 48 Xtal. Moreover, kindly tell me time for which controller stay on Ready and Lock State, when these states are used as transient states with 48 Mhz Xtal.

Regards

Saurabh Jain

This topic has been closed for replies.

1 reply

Nickname1920_O
Visitor II
Oct 10, 2014 9:40 AM UTC
Posted on October 10, 2014 at 11:40

Hello!

In Table 20 of the Datasheet the transition times are reported for the 52 MHz crystal (that means 26 MHz for the digital part). The same times for a 48 MHz crystal (that means 24 MHz for the digital part) are just slightly slower. As a rule of thumb, given the time for the 52 MHz crystal, you could consider to multiply those times by 24/26 to obtain the values for the 48 MHz crystal.

Regards!