Skip to main content
steport
Associate
Nov 26, 2014 4:56 PM UTC
Question

Spirit1 stuck in PM_setup state (0x3B)

Posted on November 26, 2014 at 17:56

Hello,

I try to set up a spirit1 device. I use your given Spiriti1 library and the example projects, but while radiInit, my device stuck everytime on the same point:

SpiritCmdStrobeLockTx();
do{
SpiritRefreshStatus();
}while(g_xStatus.MC_STATE != MC_STATE_LOCK);

This piece of code is located in the

SpiritManagementWaVcoCalibration(void)

function (SPIRIT_Management.c), which gets called during

SpiritRadioInit(&radio);

Instead of going into lock state, the device remains in PM_setup state (0x3B). Do you now why the device behaves like this? However, here is my SRadioInit config:

#define XTAL_FREQUENCY 52000000
#define SPIRIT_VERSION SPIRIT_VERSION_3_0
#define USE_MIDDLE_BAND
#define XTAL_OFFSET_PPM 0
#ifdef USE_VERY_LOW_BAND
#define BASE_FREQUENCY 0e6
#endif
#ifdef USE_LOW_BAND
#define BASE_FREQUENCY 0e6
#endif
#ifdef USE_MIDDLE_BAND
#define BASE_FREQUENCY 40e6
#endif
#ifdef USE_HIGH_BAND
#define BASE_FREQUENCY 80e6
#endif
#define CHANNEL_SPACE 20e3
#define CHANNEL_NUMBER 0
#define MODULATION_SELECT FSK
#define DATARATE 38400
#define FREQ_DEVIATION 20e3
#define BANDWIDTH 100E3
#define POWER_DBM 6
#define RSSI_THRESHOLD 0x20
/** SPIRIT Radio configuration struct */
static SRadioInit radio;
radio.nXtalOffsetPpm = XTAL_OFFSET_PPM;
radio.lFrequencyBase = BASE_FREQUENCY;
radio.nChannelSpace = CHANNEL_SPACE;
radio.cChannelNumber = CHANNEL_NUMBER;
radio.xModulationSelect = MODULATION_SELECT;
radio.lDatarate = DATARATE;
radio.lFreqDev = FREQ_DEVIATION;
radio.lBandwidth = BANDWIDTH;

#radioinit #lock #state #spirit1
This topic has been closed for replies.

8 replies

Nickname1920_O
Visitor II
Nov 27, 2014 9:02 AM UTC
Posted on November 27, 2014 at 10:02

Hello,

to be able to aswer to your question, we need more information, and to start:

  1. are you using our evaluation board?
  2. which frequency band you are working with?
  3. what crystal are you using?
Regards,

Gaetano

steport
steportAuthor
Associate
Nov 27, 2014 12:21 PM UTC
Posted on November 27, 2014 at 13:21

Hello,

Thank you for your answer.

I'm using your Spirit1 chip and radio circuit from your eval board attached to my custom board. http://www.st.com/web/en/catalog/tools/PF253894

I'm working on 433MHz frequenzy and the I have Spirit eval boards with 50MHz or 52MHz crystal. The described problems happens with both crystal frequency.

Best regards

Nickname1920_O
Visitor II
Nov 27, 2014 1:37 PM UTC
Posted on November 27, 2014 at 14:37

Hello,

do you call the following:

SpiritRadioSetXtalFrequency(XTAL_FREQ);

before radio init?

(obviusly XTAL_FREQ is 50000000 or 52000000 according to your xtal).

PS: http://www.st.com/web/en/catalog/tools/PF253894 links to a 315MHz board. Is this link correct, given that you are working at 433MHz?

Regards,

Gaetano

steport
steportAuthor
Associate
Nov 28, 2014 7:47 AM UTC
Posted on November 28, 2014 at 08:47

Hello,

Yes, I do call SpiritRadioSetXtalFrequency(XTAL_FREQ); before init. and I change the XTAL_FREQ according to my crystal. The modulues working on 433Mhz, the according resistor is set. Here is my init code:

void rfProtocolInit(void){
uint32_t i;
rf_protocol_state = Init;
//Resets Spirit1
SpiritEnterShutdown();
for(i=0;i<100000;i++);
SpiritExitShutdown();
for(i=0;i<100000;i++);
/** \brief SPIRIT Gpio configuration. */
gpio0.xSpiritGpioIO = SPIRIT_GPIO_0;
gpio0.xSpiritGpioMode = SPIRIT_GPIO_MODE_DIGITAL_OUTPUT_LP;
gpio0.xSpiritGpioPin = SPIRIT_GPIO_DIG_OUT_IRQ;
gpio1.xSpiritGpioIO = SPIRIT_GPIO_0;;
gpio1.xSpiritGpioMode = SPIRIT_GPIO_MODE_DIGITAL_OUTPUT_LP;
gpio1.xSpiritGpioPin = SPIRIT_GPIO_DIG_OUT_SYNC_DETECTED;
SpiritGpioInit(&gpio0);
SpiritGpioInit(&gpio1);
/** \brief SPIRIT Radio configuration */
radio.nXtalOffsetPpm = XTAL_OFFSET_PPM;
radio.lFrequencyBase = BASE_FREQUENCY;
radio.nChannelSpace = CHANNEL_SPACE;
radio.cChannelNumber = CHANNEL_NUMBER;
radio.xModulationSelect = MODULATION_SELECT;
radio.lDatarate = DATARATE;
radio.lFreqDev = FREQ_DEVIATION;
radio.lBandwidth = BANDWIDTH;
SpiritRadioSetXtalFrequency(XTAL_FREQUENCY);
SpiritRadioInit(&radio);
/** \brief SPIRIT package configuration */
packet.xPreambleLength = PKT_PREAMBLE_LENGTH_04BYTES;
packet.xSyncLength = PKT_SYNC_LENGTH_4BYTES;
packet.lSyncWords = 0xABCDEF;
packet.xFixVarLength = PKT_LENGTH_VAR;
packet.cPktLengthWidth = 6; //log2(MAXPAYLOADLENGTH+1) = log2(64) = 6
packet.xCrcMode = PKT_CRC_MODE_8BITS;
packet.xControlLength = PKT_CONTROL_LENGTH_0BYTES;
packet.xAddressField = S_DISABLE;
packet.xFec = S_DISABLE;
packet.xDataWhitening = S_DISABLE;
addresses.cBroadcastAddress = 255;
addresses.cMulticastAddress = 100;
addresses.cMyAddress = MyAddress;
addresses.xFilterOnBroadcastAddress = S_ENABLE;
addresses.xFilterOnMulticastAddress = S_DISABLE;
addresses.xFilterOnMyAddress = S_DISABLE;
SpiritPktBasicInit(&packet);
SpiritPktBasicAddressesInit(&addresses);
/** \brief SPIRIT IRQ configuration. */
spiritirq.IRQ_RX_DATA_READY = S_ENABLE;
SpiritIrqInit(&spiritirq);
}

and these are the definitions in the header file:

/** \brief Spirit tranceiver defines */
#define XTAL_FREQUENCY 52000000
#define SPIRIT_VERSION SPIRIT_VERSION_3_0
#define USE_MIDDLE_BAND
#define XTAL_OFFSET_PPM 0
#ifdef USE_VERY_LOW_BAND
#define BASE_FREQUENCY 0e6
#endif
#ifdef USE_LOW_BAND
#define BASE_FREQUENCY 0e6
#endif
#ifdef USE_MIDDLE_BAND
#define BASE_FREQUENCY 40e6
#endif
#ifdef USE_HIGH_BAND
#define BASE_FREQUENCY 80e6
#endif
#define CHANNEL_SPACE 20e3
#define CHANNEL_NUMBER 0
#define MODULATION_SELECT FSK
#define DATARATE 38400
#define FREQ_DEVIATION 20e3
#define BANDWIDTH 100E3
#define POWER_DBM 6
#define RSSI_THRESHOLD 0x20
/** SPIRIT Gpio configuration structs */
static SGpioInit gpio0, gpio1;
/** SPIRIT IRQ configuration struct */
static SpiritIrqs spiritirq = {0};
/** SPIRIT BasicPacket configuratuin struct */
static PktBasicInit packet;
static PktBasicAddressesInit addresses;
/** SPIRIT Radio configuration struct */
static SRadioInit radio;

Best regards
Nickname1920_O
Visitor II
Nov 28, 2014 2:46 PM UTC
Posted on November 28, 2014 at 15:46

Hello,

we have used your code with our daughter board but the issue was not reproduced.

Can you report the value of the registers f0 and f1?

Regards,

Gaetano

steport
steportAuthor
Associate
Dec 1, 2014 12:47 PM UTC
Posted on December 01, 2014 at 13:47

Hello,

I've read all Spirit registers before radioInit() and on failure I read it again. Therefore it's possible to check the register access. I observed many data conversions and probably there it fails.. I'm checking this. Here is my report:

Spirit Register Log 
before init (status ready) while initRadio() fails 
Reg Hex Dec Reg Hex Dec 
00 0C 012 00 07 007 
01 C0 192 01 40 064 
02 A2 162 02 00 000 
03 A2 162 03 A2 162 
04 A2 162 04 A2 162 
05 0A 010 05 0A 010 
06 00 000 06 00 000 
07 A3 163 07 31 049 
08 0C 012 08 0C 012 
09 84 132 09 7D 125 
0A EC 236 0A 89 137 
0B 51 081 0B CB 203 
0C FC 252 0C 0D 013 
0D A3 163 0D A3 163 
0E 00 000 0E 00 000 
0F 00 000 0F 00 000 
10 03 003 10 03 003 
11 0E 014 11 0E 014 
12 1A 026 12 1A 026 
13 25 037 13 25 037 
14 35 053 14 35 053 
15 40 064 15 40 064 
16 4E 078 16 4E 078 
17 00 000 17 00 000 
18 07 007 18 07 007 
19 00 000 19 00 000 
1A 83 131 1A 83 131 
1B 1A 026 1B 0A 010 
1C 45 069 1C 45 069 
1D 23 035 1D 23 035 
1E 48 072 1E C8 200 
1F 18 024 1F 00 000 
20 25 037 20 25 037 
21 E3 227 21 E3 227 
22 24 036 22 24 036 
23 58 088 23 58 088 
24 22 034 24 22 034 
25 62 098 25 62 098 
26 8A 138 26 8A 138 
27 05 005 27 05 005 
28 00 000 28 00 000 
29 00 000 29 00 000 
2A 00 000 2A 00 000 
2B 00 000 2B 00 000 
2C 00 000 2C 00 000 
2D 00 000 2D 00 000 
2E 00 000 2E 00 000 
2F 00 000 2F 00 000 
30 00 000 30 00 000 
31 07 007 31 07 007 
32 1E 030 32 1E 030 
33 20 032 33 20 032 
34 00 000 34 00 000 
35 14 020 35 14 020 
36 88 136 36 88 136 
37 88 136 37 88 136 
38 88 136 38 88 136 
39 88 136 39 88 136 
3A 02 002 3A 02 002 
3B 20 032 3B 20 032 
3C 20 032 3C 20 032 
3D 00 000 3D 00 000 
3E 30 048 3E 30 048 
3F 30 048 3F 30 048 
40 30 048 40 30 048 
41 30 048 41 30 048 
42 00 000 42 00 000 
43 00 000 43 00 000 
44 00 000 44 00 000 
45 00 000 45 00 000 
46 00 000 46 00 000 
47 00 000 47 00 000 
48 00 000 48 00 000 
49 00 000 49 00 000 
4A 00 000 4A 00 000 
4B 00 000 4B 00 000 
4C 00 000 4C 00 000 
4D 00 000 4D 00 000 
4E 00 000 4E 00 000 
4F 70 112 4F 70 112 
50 02 002 50 02 002 
51 00 000 51 00 000 
52 08 008 52 08 008 
53 01 001 53 01 001 
54 00 000 54 00 000 
55 01 001 55 01 001 
56 00 000 56 00 000 
57 01 001 57 01 001 
58 00 000 58 00 000 
59 03 003 59 03 003 
5A 00 000 5A 00 000 
5B 00 000 5B 00 000 
5C 00 000 5C 00 000 
5D 00 000 5D 00 000 
5E 00 000 5E 00 000 
5F 00 000 5F 00 000 
60 00 000 60 00 000 
61 00 000 61 00 000 
62 00 000 62 00 000 
63 00 000 63 00 000 
64 FF 255 64 FF 255 
65 00 000 65 00 000 
66 04 004 66 04 004 
67 00 000 67 00 000 
68 00 000 68 00 000 
69 00 000 69 00 000 
6A 00 000 6A 00 000 
6B 00 000 6B 00 000 
6C 00 000 6C 00 000 
6D 70 112 6D 00 000 
6E 48 072 6E 48 072 
6F 48 072 6F 48 072 
70 00 000 70 00 000 
71 00 000 71 00 000 
72 00 000 72 00 000 
73 00 000 73 00 000 
74 00 000 74 00 000 
75 00 000 75 00 000 
76 00 000 76 00 000 
77 00 000 77 00 000 
78 00 000 78 07 007 
79 00 000 79 00 000 
7A 00 000 7A 00 000 
7B 00 000 7B 00 000 
7C 00 000 7C 00 000 
7D 00 000 7D 00 000 
7E 00 000 7E 00 000 
7F 00 000 7F 00 000 
80 00 000 80 00 000 
81 00 000 81 00 000 
82 00 000 82 00 000 
83 00 000 83 00 000 
84 00 000 84 00 000 
85 00 000 85 00 000 
86 00 000 86 00 000 
87 00 000 87 00 000 
88 00 000 88 00 000 
89 00 000 89 00 000 
8A 00 000 8A 00 000 
8B 00 000 8B 00 000 
8C 00 000 8C 00 000 
8D 00 000 8D 00 000 
8E 00 000 8E 00 000 
8F 00 000 8F 00 000 
90 00 000 90 00 000 
91 00 000 91 00 000 
92 00 000 92 00 000 
93 00 000 93 00 000 
94 00 000 94 00 000 
95 05 005 95 05 005 
96 E8 232 96 E8 232 
97 37 055 97 37 055 
98 08 008 98 08 008 
99 08 008 99 08 008 
9A F7 247 9A F7 247 
9B 00 000 9B 00 000 
9C 00 000 9C 00 000 
9D 00 000 9D 00 000 
9E 5B 091 9E DB 219 
9F 20 032 9F 00 000 
A0 34 052 A0 00 000 
A1 11 017 A1 19 025 
A2 D6 214 A2 00 000 
A3 37 055 A3 35 053 
A4 0C 012 A4 00 000 
A5 20 032 A5 20 032 
A6 00 000 A6 00 000 
A7 E1 225 A7 E1 225 
A8 00 000 A8 00 000 
A9 01 001 A9 01 001 
AA 02 002 AA 02 002 
AB 28 040 AB 28 040 
AC 05 005 AC 05 005 
AD 83 131 AD 83 131 
AE F5 245 AE F5 245 
AF 00 000 AF 00 000 
B0 08 008 B0 08 008 
B1 00 000 B1 00 000 
B2 42 066 B2 42 066 
B3 00 000 B3 00 000 
B4 21 033 B4 21 033 
B5 10 016 B5 00 000 
B6 FF 255 B6 FF 255 
B7 00 000 B7 00 000 
B8 01 001 B8 01 001 
B9 00 000 B9 00 000 
BA 03 003 BA 03 003 
BB 03 003 BB 03 003 
BC 04 004 BC 04 004 
BD 00 000 BD 00 000 
BE 00 000 BE 00 000 
BF 00 000 BF 00 000 
C0 02 002 C0 02 002 
C1 07 007 C1 77 119 
C2 00 000 C2 00 000 
C3 00 000 C3 00 000 
C4 00 000 C4 00 000 
C5 00 000 C5 00 000 
C6 00 000 C6 00 000 
C7 00 000 C7 00 000 
C8 00 000 C8 00 000 
C9 00 000 C9 00 000 
CA 00 000 CA 00 000 
CB 00 000 CB 00 000 
CC 00 000 CC 00 000 
CD 00 000 CD 00 000 
CE 00 000 CE 00 000 
CF 00 000 CF 00 000 
D0 00 000 D0 00 000 
D1 00 000 D1 00 000 
D2 00 000 D2 00 000 
D3 00 000 D3 00 000 
D4 00 000 D4 00 000 
D5 00 000 D5 00 000 
D6 00 000 D6 00 000 
D7 00 000 D7 00 000 
D8 00 000 D8 00 000 
D9 00 000 D9 00 000 
DA 00 000 DA 00 000 
DB 00 000 DB 00 000 
DC 00 000 DC 00 000 
DD 00 000 DD 00 000 
DE 00 000 DE 00 000 
DF 00 000 DF 00 000 
E0 00 000 E0 00 000 
E1 00 000 E1 00 000 
E2 00 000 E2 00 000 
E3 00 000 E3 00 000 
E4 70 112 E4 70 112 
E5 00 000 E5 00 000 
E6 00 000 E6 00 000 
E7 00 000 E7 00 000 
E8 00 000 E8 00 000 
E9 00 000 E9 00 000 
EA 00 000 EA 00 000 
EB 00 000 EB 00 000 
EC 00 000 EC 00 000 
ED 00 000 ED 00 000 
EE 00 000 EE 00 000 
EF 00 000 EF 00 000 
F0 01 001 F0 01 001 
F1 30 048 F1 30 048 
F2 00 000 F2 00 000 
F3 00 000 F3 00 000 
F4 00 000 F4 00 000 
F5 00 000 F5 00 000 
F6 00 000 F6 00 000 
F7 00 000 F7 00 000 
F8 00 000 F8 00 000 
F9 00 000 F9 00 000 
FA 00 000 FA 00 000 
FB 00 000 FB 00 000 
FC 00 000 FC 00 000 
FD 00 000 FD 00 000 
FE 00 000 FE 00 000 
FF 00 000 FF 00 000 

Do you see any definitely wrong data? kind regards
Nickname1920_O
Visitor II
Dec 2, 2014 9:20 AM UTC
Posted on December 02, 2014 at 10:20

Hello,

I don't see anything wrong in those registers values.

The way we have reproduced your issue has been to use a board with a 26MHz crystal instead of the 52MHz one. Thus, a couple of question:

- do you use the GUI to obtain the crystal frequency? If not, how do you obtain this info?

- can you comment the call to the following function (at the end of the radioinit function):

SpiritManagementWaVcoCalibration

and report what happens.

Regards,

Gaetano

steport
steportAuthor
Associate
Dec 2, 2014 4:14 PM UTC
Posted on December 02, 2014 at 17:14

Hello,

I obtained the crystal frequency by reading the label with a magnifying glass, it's very small but readable.

I commented the SpiritManagementWaVcoCalibration function as you wrote. In my library sources, this funtion gets called in SpiritRadioSetFrequencyBase function, which gets called at the end of radioInit. (SPIRIT_Radio.c / line944).

Now the device finishes intialisation. Packet and address config works and it goes into ready state.

After initialisation i tried getting into LockTX state. I called SpiritCommandStrobes(0x66) and the device stucks in 0x3B state.

Do you have any ideas why this happens?

Thank you

Kind regards