Skip to main content
Gilberto Decaro
Associate
Jun 1, 2018 5:08 PM UTC
Question

Spirit1 strange state

Posted on June 01, 2018 at 19:08

Hi,

   During a stress test of sprit1, using the module SPSGRF 868Mhz, I've noticed an undocumented MC_STATE with value 0x41, some one know the meaning of this state ?

The module is in RX mode receiving continuously messages, occasionally appear the  0x41 state following this sequence of MC_STATE values:

33

3B

33

33

33

41

3

3

3

3

#spirit1
This topic has been closed for replies.

1 reply

balmukund66
Associate III
Jun 5, 2018 5:13 AM UTC
Posted on June 05, 2018 at 07:13

Hello ,

These are invalid state of SPIRIT1.

This indicates the Error condition in SPIRIT1.

The ERROR condition may be also due to the Error from the Host processor.

Is is possible to share more detail: About how the MC_STATE is being captured?

Thanks & Regards,

Balmukund Prasad