Skip to main content
Richard Jones
Associate II
Apr 28, 2020 2:40 PM UTC
Question

SPIRIT1 data rate at 169 MHz?

I'm looking at designing the SPIRIT1 into a new design.

The datasheet suggests up to 500 kbps (over the air), is this true for all bands, i.e. will I see 500 kbps at 169 MHz? This would make it much more appealing.

This topic has been closed for replies.

1 reply

RrW1
Associate III
Sep 29, 2020 8:11 PM UTC

Yes, you should be able to program it up to 500kbps. It is important to note that at high datarates, the communication can become unreliable. If you do plan on increasing datarate, you should also increase the amount of preamble words to make the communication more steady (i.e. 4 bytes of preamble word at 38.5kbps might be good but 4 bytes of preamble word at 150kbps might cause the receiver to miss some of the packets).