Skip to main content
wassim
Associate
Jul 4, 2014 9:43 AM UTC
Question

Spirit1 channel change delay

Posted on July 04, 2014 at 11:43

Hi,

I would like to know what is the delay when switching channels.

I am currently doing tests using the 868MHz configuration.

Regards,

Wassim
This topic has been closed for replies.

3 replies

Nickname1920_O
Visitor II
Jul 4, 2014 1:09 PM UTC
Posted on July 04, 2014 at 15:09

Hello,

can you state better your question? ETSI EN 300 200 does not prescribe a delay when switching channels.

Regards,

Gaetano

wassim
wassimAuthor
Associate
Jul 8, 2014 1:18 PM UTC
Posted on July 08, 2014 at 15:18

Hi Gaetano,

Basically we are trying to establish how long it would take to switch from one frequency to another (through the register configuration). Moreover, we would like to know if there is any ''delay'' required in this procedure in order to switch the carrier frequency.

Wassim

Nickname1920_O
Visitor II
Jul 11, 2014 11:33 AM UTC
Posted on July 11, 2014 at 13:33

Hi,

consider that it takes 54us from Ready to Tx (or Rx), without calibration, thus basically this is the time requested to pass from a frequency to another. This is true if the frequency you are passing to is near (e.g. 100kHz) the previous, and thus no further calibration is required. Instead, if the two frequencies are more far apart, calibration is needed and you have to add the related time, that is another 50us.

Regards,

Gaetano