Skip to main content
Altamash Abdul Rahim
Associate III
Jan 7, 2019 6:18 PM UTC
Question

SPBTLE-1s Example Project Run

Hello,

I am evaluating SPBTLE-1s module. I am working on a example project provided by the BlueNRG-1_2 DK 3.1.0 (remote control). The project build on truestudio and is burned on chip via st link utility. Application success messages prints on the serial terminal but no module is discoverable on my android phone. I'm using BlueNrg android app.

Note: for Spbtle-1s i have changed the preprocessor macro from 16MHz external clock to 32MHz.

Thanks.

This topic has been closed for replies.

1 reply

alok
Visitor II
Jan 13, 2019 7:01 AM UTC

Kindly try another project like Beacon, which is simple to test