Some aci commands returning timeout status from BlueNRG-MS
- 5 replies
- 1549 views
Hi All,
I am using ST's BlueNRG-MS SDK on an RTOS and when I try to send aci commands I get timeout status in return for some of them. For example in one application I am getting timeout after calling aci_gatt_add_char(), and in another example I am getting timeout for aci_hal_write_config_data().
Debugging Results:
Please find attached hci.c file for the discussion below:
1. In the
hci_send_req()
function of attached hci.c file, if I suspend the current task for very small time after callinghci_send_cmd()
at line 227 by callingnu_sleep()
in case of my OS, there is no timeout and command completes successfully.2. Similarly, instead of suspending the task as stated above, if I remove
Disable_SPI_IRQ()
call at line 271 in attached hci.c file, there is no timeout and aci command completes successfully.It is requested to please suggest a suitable and reliable solution for this problem as the above two workarounds are not reliable.
PS: I have tested the applications on firmware versions
7.1e, 7.2a and 7.2c
of BlueNRG-MS but the results are same.Regards,
Waseem Abbas
CC:
Vilei.Antonio
‌,Palmieri.Andrea
‌,Batek.Miroslav
‌,puel.bernard
‌#bluerng-ms #ble