Skip to main content
Ciuffoly
Senior
Nov 27, 2019 2:23 PM UTC
Question

[SOLVED] Use the I2C inside TouchGFX application

Is there an example to see how to use the I2C inside a TouchGFX application ?

I have found the following functions but how to select the target I2C port because

I have 4 i2C ports on my 32F746G-DISCO.

I don't know which is the I2C port number for the CN2 connector.

I2C_HandleTypeDef i2c_handler;

I2Cx_Init(&i2c_handler);

I2Cx_WriteData(0x20), 0x11, 0x00);

    This topic has been closed for replies.

    2 replies

    Ciuffoly
    CiuffolyAuthor
    Senior
    Nov 27, 2019 7:11 PM UTC

    Found the solution, add in the file stm32746g_discovery.c these functions and the relative declaration in stm32746g_discovery.h (...\Drivers\BSP\STM32746G-Discovery).

    void BSP_I2C_Init()

    {

    #define I2C_ADDRESS       0x3c

    #define I2C_TIMING     0x00B1112E

     hi2c1.Instance = I2C1;

     hi2c1.Init.Timing = I2C_TIMING;

     hi2c1.Init.OwnAddress1 = I2C_ADDRESS;

     hi2c1.Init.OwnAddress1 = 0x78; // an unused address

     hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

     hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

     hi2c1.Init.OwnAddress2 = 0;

     hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

     hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

     I2Cx_Init(&hi2c1);

    }

    void BSP_I2C_Write(uint8_t Addr, uint8_t Reg, uint8_t Value)

    {

     I2Cx_WriteMultiple(&hi2c1, Addr, (uint16_t)Reg, I2C_MEMADD_SIZE_8BIT, (uint8_t*)&Value, 1);

    }

    Ciuffoly
    CiuffolyAuthor
    Senior
    Nov 28, 2019 9:18 AM UTC

    The first fuction will be called in the screen file Screen1View.cpp

    void Screen1View::setupScreen()

    {

       #ifdef SIMULATOR

            printf("LED on\n");

       #else

            BSP_LED_Init(LED_GREEN);

            BSP_I2C_Init();

            BSP_I2C_Write(0x20, 0x11, 0x00);

       #endif

    and the other function in the relative action

    void Screen1View::buttonOPTClicked()

    {

       touchgfx_printf("buttonOPTClicked \n");

       #ifdef SIMULATOR

            printf("OPT\n");

       #else

            BSP_I2C_Write(0x20, 0x04, 0x30 + 1);

       #endif

       buttonPCM.invalidate();

    }