Skip to main content
AKuma.42
Associate
Mar 29, 2022 1:24 PM UTC
Solved

[Solved] : USBLC6-4SC6. I have checked for the operating temperature in datasheet but I could not find the same. May I know the operating temperature and Reverse Standoff Voltage and Working Voltage for the mentioned part number.

..

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 29, 2022 1:54 PM UTC

    Welcome, @AKuma.42​, to the community!

    perhaps you have overlooked the data, which is of course included in the data sheet of the USBL6-4SC6, page 2, table 1 and 2:

    • Tj (Operating junction temperature range) -40...+125 °C
    • VBR (Breakdown voltage between VBUS and GND @IR=1mA) 6...10 V

    The USBLC6-4SC6 was developed for USB 1.1 and USB 2.0, so it can protect the 5V lines commonly used there.

    Does it answer your questions?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    6 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 29, 2022 1:54 PM UTC

    Welcome, @AKuma.42​, to the community!

    perhaps you have overlooked the data, which is of course included in the data sheet of the USBL6-4SC6, page 2, table 1 and 2:

    • Tj (Operating junction temperature range) -40...+125 °C
    • VBR (Breakdown voltage between VBUS and GND @IR=1mA) 6...10 V

    The USBLC6-4SC6 was developed for USB 1.1 and USB 2.0, so it can protect the 5V lines commonly used there.

    Does it answer your questions?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    AKuma.42
    AKuma.42Author
    Associate
    Mar 29, 2022 2:31 PM UTC

    Hi Peter,

    Thanks for your response.

    Need one clarification whether Operating junction temperature and Operating temperature is same or it's different. If it's same this is the answer for my question. If not then need to know the same.

    Thanks,

    Arun

    Peter BENSCH
    ST Technical Moderator
    Mar 29, 2022 2:36 PM UTC

    The ambient temperature is important for components where power dissipation occurs and self-heating takes place. With these protection diodes, this (usually) only happens in the case of protection and only lasts for an extremely short time, so that no significant heating occurs.

    In this respect, the junction temperature can be equated with the ambient temperature.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.