Skip to main content
CChon.0
Associate II
Sep 6, 2019 6:59 AM UTC
Question

Sigfox_CLI_Demo_Project command values for start_continuous_transmission

I am trying to trigger the start_continuous_transmission for the sigfox CLI demo but it returns an error 0x0058 when I debug. What are the values to trigger it ? I tried editing the code to fit in the frequency manually but it still returns an error.

void SIGFOX_API_start_continuous_transmission_Action(void)
{
 sfx_u32 frequency=(uint32_t)920800000; //(uint32_t)unsignedCommandArgument(0);
 sfx_modulation_type_t mode=(sfx_modulation_type_t)0; 
 //unsignedCommandArgument(1); 
//0 for unmodulated 
 sfx_error_t err;
 
 err=SIGFOX_API_start_continuous_transmission(frequency, mode);
 
 responsePrintf("{&N API call...&tx}\r\n",
		 "SIGFOX_API_start_continuous_transmission", "sfx_error", err);
}

I couldn't find the parameters in the documentation or code. Please help.

Thank you

Best regards,

Chong

    This topic has been closed for replies.

    2 replies

    Thomas LB
    Associate III
    Feb 6, 2020 3:16 PM UTC

    Hi,

    I know it's late but I've searched for it for 5min so maybe it will be helpful for someone:

    just type:

    start_continuous_transmission 868000000 0

    read UM2169 for details (https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/8d/9a/ea/d7/62/06/43/ce/DM00361540/files/DM00361540.pdf/jcr:content/translations/en.DM00361540.pdf)

    Thomas LB
    Associate III
    Feb 10, 2020 9:27 AM UTC

    This morning a reproduced the sfx_error:58

    If you do

    "node_open" before "start_continuous_transmission 868000000 0" you got error 58

    just don't do "node_open" and your good