Skip to main content
Associate
Oct 13, 2023 10:37 AM UTC
Solved

Setting Cs periodically while using Dma

Good Day

I am using Spi with Dma. When using the Hal-function "HAL_SPI_Receive(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)", I want to receive 1000 times Data , which I can set in the size-area. The Problem is that my Spi-peripheral needs constantly Cs-pin to get set and reset to give out Data, else i receive after one usable data just zeros. My question is following: Is there a way to tell the Spi to set and reset the cs when data gets received, and if so, how, or where can this be configured? I am currently using the function in a for loop to receive my Data with the size set to 1. But this is way to slow. Thanks for Helping.

 

 

This topic has been closed for replies.
SquidwardBest answer
Associate
Oct 31, 2023 10:19 AM UTC

So I could solve the Problem. It is simple as that. I am using the NSSP mode wit 2 cycles in Master Inter Data Idleness

6 replies

TDK
Oct 13, 2023 7:58 PM UTC

The typical way is to handle CS as a GPIO pin, set it low prior to starting the call and set it high in the RxComplete callback. Or if you're using blocking functions, immediately after HAL_SPI_Receive.

Some series like the STM32H7 have the capability to do this natively.

Why do 1000x loops of 1 byte instead of a single call with 1000 bytes?

"If you feel a post has answered your question, please click ""Accept as Solution""."
SquidwardAuthor
Associate
Oct 16, 2023 8:19 AM UTC

First of all, thank you TDK,

The Problem is that I have to redo the function in a for, or while loop is that my SPI-Peripheral needs for every data to be send a CS high and low, or else the ADC does not get the information for giving out data. Thats why I want to find out if threr is a way to set CS high and low every time a value gets transmitted, when getting 1000 Bytes by calling this function only once.

 

AScha.3
Super User
Oct 16, 2023 8:53 AM UTC

still no info, what cpu you use ...

ie on H563 u could use TI mode : (if this is, what you want)

AScha3_0-1697446359637.png

SS = CS output

If you feel a post has answered your question, please click on " Best Answer ".
SquidwardAuthorBest answer
Associate
Oct 31, 2023 10:19 AM UTC

So I could solve the Problem. It is simple as that. I am using the NSSP mode wit 2 cycles in Master Inter Data Idleness