Skip to main content
RADS1
Associate II
Feb 28, 2017 3:18 PM UTC
Question

Sensortile BlueNRG-MS Custom Service ACI

Posted on February 28, 2017 at 16:18

Hi,

I am working on Sensortile kit with the BlueNRG-MS radio.

As per ST document PM0237 section 3.3, pg 55/99, following commands are used to add custom service to BLE device :

//Add the service with service_uuid 128bits UUID

aci_gatt_add_serv(UUID_TYPE_

128, service_uuid, PRIMARY_SERVICE,

7

,&ServHandle);

//Add the characteristic with charUuid_1 128bits UUID

aci_gatt_add_char(ServHandle, UUID_TYPE_128, charUuid_1, 20,

CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE, 0,16, 1, &CharHandle_1);

//Add the characteristic with charUuid_2 128bits UUID

aci_gatt_add_char(ServHandle, UUID_TYPE_128, charUuid_2, 20,

CHAR_PROP_WRITE|CHAR_PROP_

WRITE_WITHOUT_RESP, ATTR_PERMISSION_NONE,

GATT_NOTIFY_ATTRIBUTE_WRITE,

16, 1, &CharHandle_2);

In above 7 indicates the maximum number of attribute records that can be added to this service. However, as per my understanding BlueNRG-MS always adds 6 mandatory attribute records in any custom service. So for above example, the maximum number of attribute records would be :

6(mandatory attribute records) + 1 (charUuid_1 attribute) + 1 (charUuid_2 attribute) = 8 attribute records

What is incorrect in the above calculated value of 8 as the maximum number of attribute records ? As 7 is used as the maximum number of attribute records in above example.

Any help on above would be appreciated.

    This topic has been closed for replies.