Skip to main content
AEspo.1
Associate
Feb 29, 2020 12:27 PM UTC
Question

SensorDemoBLESensors from Cube MX 5.6.0 seems not working

I followed the "X CUBE BLE1 for STM32CubeMX" webinar/tutorial as well as the documentation in CubeMX, but my STMF401RE with IDB05A1 is not found by the ST BLE Sensor app. Hence, no connection is possible and I cannot try the Bluetooth features.

The differences with the webinar, as far as I know, are:

* I am using X.CUBE-BLE1 5.0.0 instead of 4.4.0 because this is the only compatible package with CubeMX 5.6.0.

* SYS is appearing in my system view, while it is not appearing in the webinar, but this should be again related to the new version of CubeMX

* I am using IAR EWARM instead of Eclipse (this should be super-ininfluent)

* in Advanced Setting of Project Manager, instead of "MX_USART2_UART_Init" + "MX_SPI1_Init" + "MX_X_CUBE_BLE1_Init" + "MX_X_CUBE_BLE1_Process", there are "MX_BlueNRG_MS_Init" + "MX_BlueNRG_MS_Process", and they cannot be set static

I made no modification to the generated code. I also tried the SensorDemo with BlueNRG app, but the same problem is present.

How can I fix that?

    This topic has been closed for replies.

    1 reply

    AEspo.1
    AEspo.1Author
    Associate
    Mar 6, 2020 4:38 PM UTC

    solved, at the end the problem was my phone... the app still doesn't see the device, but other bluetooth devices do

    I leave the topic open in case someone has the same problem