Skip to main content
Silas Valera
Senior
Nov 4, 2017 6:07 PM UTC
Question

S2-LP transceiver kit - STEVAL FKI868V1 - can we use balun

Posted on November 04, 2017 at 19:07

Hi 

I received 2 of this kit, and I ran some basic tests - works really fine!

I am trying to use S2-LP in wm-bus solution for my project. I have a question regarding redudcing the capacitors/inductors count on the PCB : is there any chance to use balun (say with a freq range of 

850MHz ~ 915MHz 

 (

https://cdn.anaren.com/product-documents/Xinger/BalunTransformers/B0809J50ATI/B0809J50ATI_DataSheet(Rev_A).pdf

) ? And if yes, how would that change the circuit ? 

Thanks in advance!!

Silas

#s2-lp
This topic has been closed for replies.

5 replies

indar singhal
ST Employee
Nov 7, 2017 4:43 PM UTC
Posted on November 07, 2017 at 17:43

Hi Silas,

Good to hear that you are using S2LP device.

We are currently integrating the Balue (BALF-SPI2-01D3) with S2-LP and making new Nucleo expansion board. We are validating the first prototype. S2LP package will be available on ST.com by end of Q4 or early Q1.

Meanwhile, please referrer the piece of schematic below which may be useful for you.

BR,

Indar

________________

Attachments :

S2LP_with_Balun.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyKa&d=%2Fa%2F0X0000000b66%2FLsGvNaOulQR1uhS_EJ52xAqzQwqmm0_bbKrelrOmIHI&asPdf=false
Silas Valera
Senior
Nov 8, 2017 12:31 AM UTC
Posted on November 08, 2017 at 00:31

Hi Indar, 

Thank you so much for your reply and the schematic with balun, this really reduces the component count and simplifies the design!  

Well, further looking up more information on this particular balun you mentioned, it seems this is an ST product and specifically customized for S2-LP !!!! Wonderful!! And the data sheet is also available (

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/e9/ff/cd/1e/4f/dd/49/b4/DM00417488/files/DM00417488.pdf/jcr:content/translations/en.DM00417488.pdf

) with the schematic!!  I am sure the schematic must have been tested. 

One more question:

Can we do this schematic on two-layer pcb? Or do I need to do 4 layer?

Thanks again,

Silas 

Silas Valera
Senior
Nov 22, 2017 3:14 AM UTC
Posted on November 22, 2017 at 04:14

Hello 

Anyone has worked with this balun (

BALF-SPI2-01D3) with S2-LP? I would really appreciate any information on the schematic given in the datasheet of the balun. I am planning on using S2-LP and possibly with this balun. 

Thanks in advance!!

Silas