Skip to main content
Pieter Conradie
Associate III
October 6, 2020
Solved

S2-LP: Correct procedure to change frequency?

  • October 6, 2020
  • 1 reply
  • 973 views

Hi there!

What is the correct procedure to change the S2-LP's frequency after it has been initialized with a call to S2LP_RADIO_Init()?

After I call S2LP_RADIO_SetFrequencyBase() the S2-LP appears to lock up. MC_STATE1 = 0x52 and MC_STATE0 = 0x29 which means that the state value is an invalid value of 0x14 which indicates an error condition or hardware issue.

Thanks in advance,

Pieter

https://piconomix.com

This topic has been closed for replies.
Best answer by Pieter Conradie

Apologies!! This is a bit embarrassing but the problem was between keyboard and chair :(

I tried to set the frequency to 869,000 Hz instead of 869,000,000 Hz. It's working perfectly now.

Regards,

Pieter

1 reply

Pieter Conradie
Pieter ConradieAuthorBest answer
Associate III
October 7, 2020

Apologies!! This is a bit embarrassing but the problem was between keyboard and chair :(

I tried to set the frequency to 869,000 Hz instead of 869,000,000 Hz. It's working perfectly now.

Regards,

Pieter