Skip to main content
KrunalChauhan
Associate II
Nov 19, 2019 1:02 PM UTC
Question

Query Regarding TESEO-LIV3F module. 1.Does TESEO-LIV3F provide location/Geofence Event in Basement ? If yes ,what is Accuracy ? 2.What is the process time to get the response of configurable area command ? 3.Can it support up to 200 configurable area

We want to develop our Product in which want to use TESEO-LIV3F Chip but still we have some query so please provide proper answer quickly.

1. Does TESEO-LIV3F provide location/Geofence Event in Basement ? If yes then what is the accuracy of it ?

2. As per Datasheet "Teseo-LIV3F receiver supports at least 8 circular areas where 4 circular areas are configurable in the firmware" it supports 4 configurable area but, we need to check total 200 area using our product so can we use this chip?

3. What is the process time to get the response of configurable area command ?

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Nov 19, 2019 3:42 PM UTC

    GPS/GNSS signals don't penetrate buildings/structures well, this is usually achieved via the kinetic part of the delivery system.

    With 200 areas you're probably going to need to code/optimize your own solution with a micro-controller. Depending on your merit as a customer you might have access to an application layer where you can implement your own algorithm. Circles tend to be use as there are good optimization and computation reduction methods.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    KrunalChauhan
    Associate II
    Nov 20, 2019 4:52 AM UTC

    Thanks for reply.

    What is the process time to get the response of configurable area command ?