Skip to main content
Associate
Sep 26, 2023 1:02 AM UTC
Question

NUCLEO-H743ZI2

Hello Everyone!

I think it's a weird question, however, I am new to NUCLEO-H743ZI2.  Actually, I am facing the issue of low-speed data transfer from MCU to PC (LabVIEW). Before, I was using programming and debugging USB ports to transfer data to LabVIEW. However, I was only able to transfer at a maximum of 115200bps (14400 Bytes ps). Although my requirement is 50,000 Bytes per sec. 

Then I found the USB OTG_FS Connector (CN13). However, I am not sure about the maximum speed through which I can transfer data. And what about the Ethernet port (CN14)? 

This topic has been closed for replies.

1 reply

TDK
Sep 26, 2023 1:48 AM UTC

The UART port should be capable of 921600 or more. Increasing baud rate is probably the easiest solution here.

USB FS can transfer around 5 Mbps, but is more complicated to program.

Eithernet faster than USB FS, unsure of the max but at least 10s of Mbps.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."