Skip to main content
Skuma.7
Associate
Sep 15, 2020 12:49 PM UTC
Question

Not able to read RSSI value between two bluenrg bluetooth unit

Hi,

To measure distance between two bluenrg module using rssi value.

The two devices are loaded with BLE_Beacon example with different public address and few scanning functions are included.

Both the device advertising data can be seen in ST Ble APP in the mobile.

But at the device side,to scan and read the rssi value,the "hci_le_advertising_report_event()" event function is not invoked during scanning.

Advertising is working ,but scanning is not work at device side.

Board:STEVAL-BCN002V1B - (BlueTile)

Thanks in advance.

This topic has been closed for replies.

7 replies

Eleon BORLINI
ST Employee
Sep 15, 2020 3:22 PM UTC

Hi @Community member​ ,

please check if this thread on a similar topic can be of any help for you.

-Eleon

Skuma.7
Skuma.7Author
Associate
Sep 16, 2020 1:48 AM UTC

Hi,

Thanks for your reply.

The above thread seems to be focusing on Mesh network and its corresponding functions.

But i am using software pack"STSW-BLUETILE-DK 1.3.0" which is not a mesh functionality just advertising and scanning functionality between the devices.

I referred the below link document for my application development and followed the procedure as per that document.

https://www.st.com/resource/en/application_note/dm00712091-social-distancing-detection-using-bluetooth-low-energy-stmicroelectronics.pdf

As per the above document, the "hci_le_advertising_report_event()" event function is not invoked during scanning.

So i am not able to collect the RSSI value of each node during scanning.

Thanks in advance.

Eleon BORLINI
ST Employee
Sep 25, 2020 10:39 AM UTC

Hi @Community member​ 

If you are still facing the issue, I've added BLE-related topics for more support.

-Eleon