Skip to main content
jp1
Associate II
Mar 28, 2016 7:43 AM UTC
Question

Need GPIO to Disable External HSE for 32L4 in X-CUBE-BLE1

Posted on March 28, 2016 at 09:43

Hi,

We're using Nucleo-L4 with X-CUBE-BLE1 Expansion SW with lower mode enabled.

The 32L4 HSE XTAL input is driven by external oscillator.

We would like to disable the external clock during low power mode of 32L4 and enable when 32L4 comes out of low power mode. Is three a way to do this via a GPIO pin of 32L4 ? if so, any guidance will be appreciated.

Thanks.

#stm32l4-external-hse-x-cube-ble1 #stm32l4-ble-expansion-lpm-stop
This topic has been closed for replies.

3 replies

jp1
jp1Author
Associate II
Apr 5, 2016 7:05 AM UTC
Posted on April 05, 2016 at 09:05

More specifically, should we disable the external HS lock via GPIO before calling LPM_Enter_Mode or from within this function?

Should we enable the external HS clock from within or outside of function call:

:LPM_ExitStopMode()?

Thx,

jp1
jp1Author
Associate II
Apr 12, 2016 7:06 AM UTC
Posted on April 12, 2016 at 09:06

An update... After some more digging we were able to locate the section which enters STOP mode: HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI).

For the case when it exists STOP mode is not straightforward.  The following LPM_EnterStopMode() function hints at the LPM_ExitStopMode() as the logical entry point for a GPIO toggle:

void LPM_Enter_Mode(void)

{

    uint32_t uwPRIMASK_Bit;

    uwPRIMASK_Bit = __get_PRIMASK();    /**< backup PRIMASK bit */

    __disable_irq();            /**< Disable all interrupts by setting PRIMASK bit on Cortex*/

        

    if(uwRUN_Req == 0)

    {

        if(uwDeepSleep_Req)

        {

            /**

             * Enter Sleep Mode

             */

            HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);

        }

        else if (uwPDDS_Req == 0) /* WARNING: This mode is not supported yet by any platform */

        {

            LPM_EnterStandbyMode();    /**< Call user Hook */

            /**

             * Clear Wakeup flag

             */

            __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

            /**

             * Enter Standby Mode

             */

            HAL_PWR_EnterSTANDBYMode();

            LPM_ExitStandbyMode();    /**< Call user Hook */

        }

        else

        {

            /**

             * Clear Wakeup flag

             */

            __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

            /**

             * Enter Stop Mode

             */

            if(uwLPSDSR_Req)

            {

                HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);

            }

            else

            {

#ifdef USE_STM32L4XX_NUCLEO      

                                HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

#else

                                HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

#endif

            }

            LPM_ExitStopMode();    /**< Call user Hook */

        }

    }

    __set_PRIMASK(uwPRIMASK_Bit);    /**< Restore PRIMASK bit*/

    return;

}

But the code never gets to that function call.  Is there another place or fucntional call we're missing?

ST Employee
Apr 25, 2016 11:47 AM UTC
Posted on April 25, 2016 at 13:47

Hello,

If the  LPM_ExitStopMode() is never called, that means you never enter STOP mode. I do not see any other reason.

Once you will be able to enter STOP Mode, LPM_ExitStopMode() is the function where to switch ON your HSE.

In the example provided, it is used similarly to switch ON the PLL.

In order to switch OFF the HSE, you should add another hook which is missing in the actual delivery.

You should implement a LPM_EnterStopMode() in which you should first switch on HSI/MSI before switching of the HSE ( assuming HSE is used as system clock for your CPU)

LPM_EnterStopMode()  shall be called just before HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI)

Regards.