Skip to main content
Associate
Aug 4, 2023 5:06 AM UTC
Solved

Need details for USB Interface IC DRP

Here I'm using a USB Interface IC DRP for OTG. when I look into the datasheet for interfacing, I find some details in the pinout contrary to the diagram for pin numbers 16 and 17. Please someone clarify in this 

AravindR_0-1691125297024.png

AravindR_1-1691125349801.png

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 4, 2023 5:48 AM UTC

Welcome @Aravind R, to the community!

Thank you very much for pointing this out! It is a typo in the numbering of the pin numbers of the TCPP03-M20 in the pin out drawing. If you look closely, you can see that

… 15 17 16 18 …

was numbered there by mistake.

Regards /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 4, 2023 5:48 AM UTC

Welcome @Aravind R, to the community!

Thank you very much for pointing this out! It is a typo in the numbering of the pin numbers of the TCPP03-M20 in the pin out drawing. If you look closely, you can see that

… 15 17 16 18 …

was numbered there by mistake.

Regards /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Aravind RAuthor
Associate
Aug 4, 2023 6:10 AM UTC

Thanks peter