Skip to main content
David Turner
Visitor II
Jan 24, 2017 12:05 AM UTC
Question

Mistake in ST3232 datasheet

Posted on January 24, 2017 at 01:05

In the

http://www.st.com/content/ccc/resource/technical/document/datasheet/group1/40/2c/7f/62/3a/3f/47/3c/CD00002253/files/CD00002253.pdf/jcr:content/translations/en.CD00002253.pdf

, the introduction text says:

The devices require only four small 0.1 mF standard external capacitors for operation from a 3 V supply.

However, Table 9 states the capacitance value as 0.1uF, a value 1000 smaller than 0.1mF.  Please could you confirm which of these is correct (I assume 0.1uF) and update the datasheet so the values agree?

David

    This topic has been closed for replies.

    1 reply

    Tamas Novak
    Associate III
    Mar 18, 2017 4:49 PM UTC
    Posted on March 18, 2017 at 17:49

    It is surely 100nF. I've used it a number of times and worked well.