Skip to main content
pmuldoon
Visitor II
Aug 15, 2016 2:48 PM UTC
Question

mini AP help

Posted on August 15, 2016 at 16:48

I'm finding very little info on how to set up the module.  Can anybody point me to some sample scripts or something?   My goal is to see the SSID with a phone/tablet/laptop and connect to it and then open a webpage on the module so I can send/receive a simple text file of data. 

So I think I want to set up as a mini AP.  I've fumbled around and found that if I change any settings I need to turn the wifi off/on to update the settings.  Right now I have an SSID that I can see with my phone, but when I connect I get the following:

+WIND:28:Station 00:34:DA:9A:1F:42 Associated:0

+WIND:72:Station 00:34:DA:9A:1F:42 Disassociated:3

and my phone hangs on ''obtaining ip address''.  The phone says it is using WEP and prompts me for a string.  I enter 5 ascii zeros and the connect button activates so I can connect, but then it hangs.  Not sure if i'm having WEP issues or DHCP issues.  Any thoughts?

I've sent these settings via Terminal:

AT+S.SCFG=wifi_mode,3        //set to miniAP mode

AT+S.SCFG=blink_led,1        //blink led for # of connects

AT+S.SCFG=ip_use_dhcp,2        //mini AP mode provides DHCP

AT+S.WIFI=0            // turn OFF wifi

AT+S.WIFI=1            // turn ON wifi

and my AT&V is:

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01SA1

#  nv_serial = 2415D36371

#  nv_wifi_macaddr = 00:80:E1:B5:9F:C1

#  blink_led = 1

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 115200

#  console1_hwfc = 0

#  console1_enabled = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 50:72:6F:69:7A:76:6F:64:6E:6A:61:20:54:65:73:74:69:72:61:6E:6A:65:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 22

#  wifi_txfail_thresh = 5

#  wifi_ht_mode = 0

#  wifi_channelnum = 11

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 3

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 2

#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 00:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 0B:B7:B0:8D:23:7A:BB:A0:B9:80:A7:58:62:4E:95:22:5B:B7:09:61:16:6D:C2:EF:AF:B3:8C:54:4B:3D:F8:E2

#  wifi_wpa_psk_text = mikroe123456

#  ip_use_dhcp = 2

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-B5-9F-C1

#  ip_apdomainname = captiveportal.net

#  ip_apredirect = firstset.html

#  ip_ipaddr = 192.168.0.50

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.0.1

#  ip_dns = 192.168.0.1

#  ip_http_get_recv_timeout = 3000

#  ip_wait_timeout = 12000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Aug 23, 2016 7:23 PM UTC
    Posted on August 23, 2016 at 21:23

    miniAP only support no security and WEP security. Set wifi_priv_mode to proper value.

    Another tip:

    - call wifi=0

    - set variables

    - call wifi=1