Skip to main content
_KSoni.3
Visitor II
Mar 8, 2022 6:25 AM UTC
Question

Migration from BlueNRG-2 to BlueNRG-LP

Hello All,

I am working on a custom board which has BlueNRG-2 IC as a connectivity chip with Mobile App. I am now planning to migrate to BlueNRG-LP IC because of memory limitation in BlueNRG-2.

Is there any migration document for the same?

Following are the components which I am currently using in BlueNRG-2:

  • UART
  • DMA
  • SPI
  • Bluetooth
  • JTAG

    This topic has been closed for replies.

    1 reply

    Sebastien DENOUAL
    ST Employee
    Mar 8, 2022 10:00 AM UTC

    Hi @_KSoni.3​ ,

    There is two aspect to consider while migrating from BlueNRG-2 to BlueNRG-LP :

    • Peripherals as you mentioned
    • BLE stack APIs.

    At first, let me say that code philosophy is the same between BlueNRg-2 and BlueNRG-LP. That means that if you are used with BlueNRG-2, BlueNRG-LP will not be a proble.

    To start, I would advise to download and install BlueNRG-LP SDK. It includes multiples code examples and some of them should already answers your needs - In my opinion, probably easier to modify those code examples for your own needs. There is also dedicated code examples for each peripherals ( UART/DMA/I2C/SP/...).

    Coming back to migration ( BLE stack migration), either you can use code example from BlueNRG-LP SDK or it exists a Migration BLE stack guidelines from v2.x to v3.x.

    In any case, whatever your approach, you should consider a code example from BlueNRg-LP SDK as basis for your development (this is easiest way in my opinion)

    This doc is part of BlueNRG-LP SDK : C:\Users\USER_NAME\BlueNRG-LP DK 1.1.0/doc/index.html

    Regards,

    Sebastien.