Skip to main content
JMill.18
Associate II
Sep 10, 2024 3:29 PM UTC
Question

Manual or tutorial for ST Customized Protocol in AN5041?

In AN5041 Rev 5, pages 26-28, there is an example programming sequence for the STEVAL-IDP004V2 master and a device on a STEVAL-IDP003V1 using ST's customized protocol (a substitute for IO-LINK).

Is there a manual or tutorial  or resource page that goes through programming the boards and communicating with them with ST's customized protocol? 

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
Sep 10, 2024 4:27 PM UTC

Hello,

Check out this video and see if you find what you are looking for.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
JMill.18
JMill.18Author
Associate II
Sep 11, 2024 6:27 PM UTC

Thank you SofLit, I have that other kit as well, the documentation is more clear to me too.

I still have the issue of what to do with my 4-port master hub since it has been programmed with the ST Customized Protocol, see AN5041 - Rev 5 page 22.  I programmed the STEVAL-IDP004V2 hub with the file  "STEVAL-IDP004V2-RS485.hex".  It seems for this setup with the STEVAL-IDP003V1, the IO-Link demo is the simpler way, but, after much searching, where is the hex file for programming the STEVAL-IDP004V2  (AN5041 - Rev 5, section 5 on page 29)?  Notice how the documentation's steps don't say what the hex file is and where to get it from.   I can't find it on ST's site, there only seems to be IO-Link libraries, but no hex file to set the board back to what it was from the factory.  Once that is done, then I can try the video you mentioned with the IO-Link Master example. 

 Where do I get the hex file for the IO-Link setup for the STEVAL-IDP004V2 hub?

 What is the process to renew the license?

Thank you,

-James