Skip to main content
Chandrashekar C
Associate III
Aug 6, 2021 10:34 AM UTC
Question

M41T62 RTC Alarm

Hello, 

We are currently using the M41T62 RTC which is connected to a STWINKT1B board from ST along with the drivers meant to be used with M41T62(download page).

We have been successfully able to use it to set a 1 min alarm with interruptions in repetitive mode. 

The same was possible with a 1-hour alarm with interruption. We followed the guidelines given for the TIMEKEEPER series application note that tells us to set RTP5, RTP4, RTP3, RTP2, and RTP1 to set the right repetitive alarms. 

The problem we have is that we are unable to set it for in-between durations such as 1 min or 30 mins or 5 mins. Can you help us out with this?

/*
Simple Test code
*/
 
M41T62_Date_st Date = { 0, 0, 0, 0, 0 };
M41T62_Time_st Time = { 0, 0, 0, 0 };
uint32_t rtcECntr = 0;
uint32_t pre_rtcECntr = 0;
M41T62_AF_State_et af = M41T62_AF_LOW;
M41T62_Alarm_st alarm = { 0, 0, 0, 0, 10 };
int ret = BSP_ERROR_NONE;
 
/*
Check for I2C Device
*/
for (int i = 1; i < 256; i++) {
 ret = HAL_I2C_IsDeviceReady(&hi2c4, (uint16_t) (i << 1), 3, 5);
 if (ret == HAL_OK) {
 msg_info("\nDevice Id = %02d", i);
 }
}
/*
Read Date/Time from STM32 internal RTC
*/
 
/* Get the RTC current Time */
HAL_RTC_GetTime(&hrtc, &start_rtctime, RTC_FORMAT_BIN);
/* Get the RTC current Date */
HAL_RTC_GetDate(&hrtc, &start_rtcdate, RTC_FORMAT_BIN);
Time.Hours = start_rtctime.Hours;
Time.Minutes = start_rtctime.Minutes;
Time.Seconds = start_rtctime.Seconds;
Time.Seconds_10Ths = start_rtctime.SecondFraction;
Date.DayMonth = start_rtcdate.Date;
Date.DayWeek = start_rtcdate.WeekDay;
Date.Month = start_rtcdate.Month;
Date.Year = start_rtcdate.Year;
 
if(M41T62_Setting_Date(Date) != M41T62_OK)
 msg_error("\nM41T62_Setting_Date()");
if(M41T62_Setting_Time(Time) != M41T62_OK)
 msg_error("\nM41T62_Setting_Time()");
 
 
alarm.AlSeconds = 0X30;
alarm.AlMinutes = 0x01;
M41T62_Get_AF_Bit(&af);
M41T62_Set_AFE_Bit(M41T62_AFE_LOW);
 
if(M41T62_Disable_Alarm() != M41T62_OK)
 msg_error("\nM41T62_Disable_Alarm()");
if(M41T62_Setting_DefaultBit() != M41T62_OK)
 msg_error("\nM41T62_Setting_DefaultBit()");
if(M41T62_Alarm_Setting(alarm) != M41T62_OK)
 msg_error("\nM41T62_Alarm_Setting()");
if(M41T62_Alarm_Repeat_Mode_Setting(M41T62_OnceperHour) != M41T62_OK)
 msg_error("\nM41T62_Alarm_Repeat_Mode_Setting()");
 
/*
Set Alarm Enable Bit
*/
M41T62_Set_AFE_Bit(M41T62_AFE_HIGH);
HAL_Delay(100);
 
 
M41T62_Get_AF_Bit(&af);
msg_info("\n\n");
 
rtcECntr = 0;
 
/*
Loop through and check for Alarm Bit
*/
while (1) {
 HAL_Delay(1000);
 M41T62_Get_AF_Bit(&af);
 if (af == M41T62_AF_HIGH) {
 msg_info("\n========> Alarm AF Set");
 ret = M41T62_Getting_Time(&Time);
 if (ret == M41T62_OK) {
 msg_info("\tTime:%02d:%02d:%02d:%02d\t%02ld\t%02lds\n", Time.Hours,
 Time.Minutes, Time.Seconds, Time.Seconds_10Ths,
 rtcECntr, (rtcECntr - pre_rtcECntr));
 pre_rtcECntr = rtcECntr;
 }
 else
 {
 msg_error("\nM41T62_Getting_Time Failed!")
 }
 } else {
 msg_info(".");
 }
 M41T62_ReadRegs(M41T62_AL_MONTHREG, 5, tmp);
 rtcECntr++;
}

Attaching below is a reference code that we are currently running.

    This topic has been closed for replies.

    5 replies

    Peter BENSCH
    ST Technical Moderator
    Aug 9, 2021 11:30 AM UTC

    The repeat modes in the M41T62 are only able to repeat once per second/minute/hour/day/month or year (datasheet, table 7). You need to reprogram the RTC after each alarm if you need different repetition time intervals.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Chandrashekar C
    Associate III
    Aug 9, 2021 11:39 AM UTC

    Hi Peter,

    Thanks for your response. I am doing that in my main application. But I can't get the M41T62 alarm to work other than once per second/minute/hour/day.

    Is it possible to share some sample working code where the M41T62 alarm is set to 5 mins, repetitive ? Please.

    Kind Regards

    Chandrashekar

    Peter BENSCH
    ST Technical Moderator
    Aug 11, 2021 9:53 AM UTC

    You can set the alarm clock to any time. However, you will have to calculate and reprogram the following alarm time every time if you need something similar to the repeat modes.

    With the generic C driver STSW-M41T62 it should be easy to reset the alarm clock.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.