Skip to main content
JEnya
Associate
Oct 11, 2019 3:00 PM UTC
Question

M41T62 not triggering on month or year repeat modes

I am using an M41T62 to test the various repeat modes using bits RPT1-RPT5. Most of the repeat modes appear to be triggering an alarm properly, with the exception of MONTH (only RPT5 set) and YEAR (RPT1-RPT5 clear).

For example, to test this, I set the time to Tues, 31 Dec 2019, 23:59:45 and configure for either MONTH or YEAR repeat mode. The date rolls over as to Wed, 1 Jan 2020 but I do not receive and IRQ and AF is not set.

I have also tried, for example, setting the date to Tues, 1 Oct 2019, 23:59:45 in case the MONTH repeat mode triggers at the end of the first day of the month.

Is there something I am missing?

    This topic has been closed for replies.