Skip to main content
Visitor II
Sep 13, 2023 9:28 AM UTC
Question

LVDS transceiver RHFLVDSR2D2 failure info

Good afternoon,

 

We are evaluating the possible consequence for the LVDS transceiver RHFLVDSR2D2 in case that it is supplied with a voltage above its absolute value which is 4,8V.

In particular we are asked to evaluate the case that voltage applied to supply is 5V: can you provide us some information to analyse this failure? Is possible to have an equivalent failure impedance to be considered from supply to inputs/output pins?

Also a very simple equivalent circuit of input/output would be very useful to analyse effects on interface in such failure case.

Kind regards

This topic has been closed for replies.

2 replies

Issamos
Super User
Sep 13, 2023 10:10 AM UTC

@FabioCamozzi76 

I don't think such evaluation exist. To do this I suggest you to test it yourself refering to the Test circuit in the datasheet of the components.

Best regards.

II

DMala.1
Associate II
Sep 13, 2023 2:14 PM UTC

Hello, I measure the output differential voltage of the drivers (with 100ohm termination resistor) and it is always higher than 0.4V that is referred to the datasheet. What I measure is about 0.68V. Is that normal? 

Thank you in advance