Skip to main content
Smalik
Associate III
Dec 26, 2023 8:13 AM UTC
Question

LSM6DSO - SPI Modes Issue

Hello,

I ordered this IC for one of my products and am confused about the SPI modes. In the datasheet, it is mentioned that it will support SPI mode 0 and mode 3, but I have not found any timing diagram of SPI mode 0 in the datasheet. Can you provide me more details about this IC How can I change the SPI modes and on which mode this IC works fine, and the timing diagram of SPI mode 0?

 

Thanks and Regards

Sarthak Malik

 

This topic has been closed for replies.

9 replies

AScha.3
Super User
Dec 26, 2023 10:04 AM UTC

SPI modes:

AScha3_0-1703583145921.png

I think, its not explained in a clear way: mode0 is 4-wire , other mode is 3-wire SPI , depends on SIM bit in ctrl3_c register.

"mode" is also used for the operating mode , so this is confusing somewhat, see:

AScha3_1-1703584409725.png

Also the interface can be in different "mode" : SPI , I2C , I3C -> depends on pin settings

AScha3_2-1703584667692.png

AScha3_3-1703585289861.png

 

 

So there is no "better" timing on SPI, just 3 or 4 wire mode can be selected, default is 4 wire SPI.

I would try this 4 wire SPI first.

 

If you feel a post has answered your question, please click on " Best Answer ".
Smalik
SmalikAuthor
Associate III
Dec 26, 2023 1:13 PM UTC

Hello,

 

Thanks for your reply. I think these are not SPI modes. These are connection modes.  I am asking about the SPI modes. In the datasheet, it is mentioned that it supports both SPI modes. Mode 0 and mode 3 as you can see in the attached screenshot.

Smalik_0-1703596292339.png

But there is no timing diagram available for SPI Mode 0.

Smalik_1-1703596357632.png

Regards

Sarthak

AScha.3
Super User
Dec 26, 2023 1:31 PM UTC

Yes, but this i tried to explain: SPI has 4 or 3 wire mode, thats it. Other is the operating mode ...3 or whatever;

(as i understand this ...)

AScha3_0-1703597174960.png

If there is a "spi-mode 0" with different timing or whatever, there is nothing about in this ds.

If you feel a post has answered your question, please click on " Best Answer ".
Smalik
SmalikAuthor
Associate III
Dec 28, 2023 9:03 AM UTC

Hello,

 

Thanks for the reply. So, is it working fine on SPI Mode 0, that is, CPOL =0 and CPHA =0? and if it is working fine, can you provide me the timing diagram of the SPI Mode 0?

 

Regards

Sarthak Malik

AScha.3
Super User
Dec 28, 2023 9:23 AM UTC

Just try the spi communication - then you know 100% sure.

AScha3_0-1703754888097.png

+ CPOL =1 and CPHA =1  --- i think,  just try it!

+ see:

https://hackaday.com/2016/07/01/what-could-go-wrong-spi/

 

If you feel a post has answered your question, please click on " Best Answer ".
Smalik
SmalikAuthor
Associate III
Dec 28, 2023 9:41 AM UTC

I know it will work fine on CPOL 1 and CPHA 1. but my concern is whether it will work on CPOL 0 and CPHA 0 or not.

 

Regards

Sarthak

AScha.3
Super User
Dec 28, 2023 9:49 AM UTC

So you just wanna play around with some settings - just for fun ?

CPOL 0 and CPHA 0 also latch data on rising clock - maybe it works - just try it.

If you feel a post has answered your question, please click on " Best Answer ".
Smalik
SmalikAuthor
Associate III
Dec 28, 2023 10:23 AM UTC

No, I do not wanna play with settings. Actually, the problem is I have another IC that is also configured on CPOL 0 and CPHA 0. So, on the same SPI line, I want to connect this IC. So that's why I want to confirm whether it will work on CPOL 0 and CPHA 0 or not.

AScha.3
Super User
Dec 28, 2023 12:11 PM UTC

Ok, so you need 2x CS to select one of the chips , setting in software a port/pin. (no hardware css)

Just set spi register (SPIxCFG2 - i think) with CPOL 0 and CPHA 0 , then do spi transfer, when using chip A , or 

set CPOL 1 and CPHA 1 then CS low for the LSMxx , then do spi transfer on this chip.

Easy, fast and will work with both chips with their correct timing/phase.

If you feel a post has answered your question, please click on " Best Answer ".